Bridgewater, New Jersey – Signify (Euronext: LIGHT), the world leader in lighting, announces new Philips Hue lights and accessories to design personalized lighting experiences. The new Philips Hue Dymera wall light offers individually controllable up and down light to create an architectural look both indoors and outdoors. In Canada, new editions of the Philips Hue Being ceiling light are also being introduced. Lastly, smart lighting is uniquely integrated with smart home security with the Philips Hue Secure starter kit and Secure floodlight camera, as well as additional app features.
Dual beam control for a sophisticated scenery
The Philips Hue Dymera wall light combines functionality and style, offering individual control over two beams of light that shine up and down. With its sophisticated black design, Dymera is suitable for both indoors and outdoors, where it can illuminate large surfaces with warm-to-cool white and color light. Using the Philips Hue app, each light can be dimmed or brightened while changing the colors individually. You can also set a scene from the scene gallery for a more cohesive look.
More flexibility for a personalized design
The Philips Hue Being ceiling light is available in black and white in addition to the existing aluminum version. With a halo of soft light around the lamp and the ability to use 50,000 shades of warm-to-cool white light, the lamp is suitable for bedrooms, hallways and entryways.
Enhancing the Philips Hue Secure system
The Philips Hue Secure camera starter kit and the Philips Hue Secure floodlight camera are now available. Suitable for both indoors and outdoors, the Philips Hue Secure starter kit is specifically designed to bring a full suite of smart home security capabilities to new users. It offers a Philips Hue Secure wired camera — which includes a power supply unit and wall mount to install the camera wherever you want — as well as two Philips Hue Secure contact sensors to send real-time notifications when the contact sensor is opened or closed. Furthermore, the starter kit includes two Philips Hue bulbs that offer warm-to-cool white and colored light and a Philips Hue Bridge, granting access to all the features that the Philips Hue Secure system has to offer. With features such as live view, night vision and two-way talk, Philips Hue Secure can send you notifications of potential security threats or scare off intruders with unique light and sound alarms.
Specifically developed for outdoor use, the previously announced Philips Hue Secure floodlight camera brings the best of the Philips Hue system together. It lets you keep an eye on the backyard, patio or driveway, and — when you trigger a light alarm from the Philips Hue app — the floodlight immediately illuminates a large area in any color, such as bright white or even red. The Philips Hue Bridge is required for the Secure floodlight camera.
Upcoming features for Philips Hue Secure
Philips Hue is continuously bringing new features to the Security Center of the Philips Hue app. New updates are expected in the first half of 2024; these include improvements to security push notifications and the event timeline, as well as automatic light and sound alarms when motion is detected. Additionally, Philips Hue is working to develop support for Amazon Alexa and Google Home for the Philips Hue Secure system.
To find out more about the latest Philips Hue products and app features, visit www.philips-hue.com/newlaunches.
Availability
Signify – Philips Hue
E-mail: philipshue@coynepr.com
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.