Markham, Canada – Signify (Euronext: LIGHT), the world leader in lighting, announces the launch of brand-new Philips Hue lights and app features that provide additional ways to expand and personalize the lighting in your home. Philips Hue Twilight, the brand’s newest innovation, was designed to support your circadian rhythm. After the launch of the Lightguide Ellipse bulb, the Philips Hue Lightguide selection is completed with four more shapes — small globe, large globe, Edison, and triangle — which can be seamlessly combined with matching table lamp bases. Also launching is the Philips Hue Solo lightstrip, which enables you to add light anywhere in your home, and Philips Hue Datura, a dual light source ceiling panel.
Wake up feeling more recharged
Philips Hue Twilight sleep and wake up light, available in both white and black, was designed to support your circadian rhythm: it helps you maintain a regular sleep routine, fall asleep peacefully, and wake up feeling more recharged. With two individually controllable light sources — an illumination head and a back light featuring one-of-a-kind ColorCast technology — Philips Hue Twilight mimics the wide palette of colors in both morning and evening sky light.
The compact design fits easily onto a bedside table and features two customizable buttons to control the light, in addition to the Philips Hue app. By default, one button cycles through six new light scenes, like ‘Arise’ or ‘Sleepy’. The other triggers the new Sunset Go to sleep automation, simulating a sunset with a rich blend of red tones.
Additionally, set a wake up automation, which gradually brightens so you gently awaken to the colors of the morning sun. Ultra-low dimming enables smooth transitions for an effective wake-up and the perfect nightlight. Philips Hue Twilight dims to an industry leading 0.5% brightness1.
An eye-catcher that complements your modern home decor
Following the launch of the popular Ellipse shape, the four new Philips Hue Lightguide bulbs allow you to create a unique lighting experience. Users can now choose from five premium shapes of handblown glass bulbs: small globe, large globe, triangle, Edison and Ellipse. Their striking and contemporary design offers eye-catching modern style along with all the smart functionalities of Philips Hue. These bulbs offer millions of shades of white and color light, so that you can personalize and design colorful light scenes, and are controllable with the Philips Hue app.
Lightguide bulbs can be combined with the Philips Hue 3D-printed table lamp base. Users can place the duo on side or coffee tables as a striking decorative piece to enrich their home décor. The lamp, which is 3D printed using bio-circular materialsii, is available in sage, sand, and glossy black.
Flexibly add light in hard-to-reach spaces
Shape and bend lighting to your needs with the Philips Hue Solo lightstrip. Easy to use and accessible for any user, it offers the flexibility to add light in even hard-to-reach places. With cuttable 3m, 5m and 10m versions, it subtly fits into any area, such as in closets, on ceilings or walls, and along stairs and floors, to upgrade any space. Illuminated by 1700 lumens of stunning light output, the lightstrip brightens your home with pure color and pure white light (thanks to RGBWWW LEDs). Philips Hue users can conveniently expand their smart lighting range by integrating the lightstrip with the full Philips Hue system — enabling different light experiences to fit any mood.
Ceiling lights to illuminate any space
Philips Hue Datura ceiling light with a round shape and slim frameless profile enhances the sense of space anywhere around your home, especially in rooms with low ceiling height. The ceiling panel comes with two individually controllable light sources in white and color light that create both room illumination, with a powerful functional light, and a soft ceiling glow with a single touch and customizable color effects.
Jasper Vervoort
Business Leader Philips Hue at Signify
Other new launches from Philips Hue
GU10, and spot luminaires that use the GU10, have been upgraded and now shine brighter, allowing you to illuminate your rooms even more. They offer 400 lumens at 4000k compared to the previous generation’s 350 lumens, Additionally, new GU10 bulbs help you take a step toward a more energy efficient smart home, with a longer lifespan of 25,000 hours (compared to 15,000 hours) and 50% lower standby power consumption.
Besides continuous innovations on lights, Philips Hue also has new app updates and improvements for its integrated security system. Philips Hue Secure users can set light and sound alarms to go off automatically when the system is armed, as well as schedule their security systems to arm and disarm automatically on a schedule. Additionally, users can select from three different battery optimization modes. New features will become available Summer 2024.
Lastly, Philips Hue is proud to announce its partnership with OnTech in North America, which seeks to make it easier for users to get Philips Hue in their homes. OnTech provides installation services for wired and non-wired Philips Hue products. Whether they don't have the time to install the lights or they would just rather leave it to the professionals, users can count on OnTech to get set up quickly.
To find out more about the latest Philips Hue products and app features, visit www.philips-hue.com/newlaunches.
Available June 18, 2024
Available in September 10, 2024
iIn a recent report by Stiftung Warentest, the organization presents findings from its evaluation of various smart LED lamps available in the European market, focusing on several performance metrics including the minimum dimming level. The findings revealed that Philips Hue products had the best dimming performance in the test.
iiThe materials used are ISCC PLUS (International Sustainability and Carbon Certification) certified waste streams and residues. These can be tall oil from the wood processing industry or used cooking oil. The bio-circular granulate used as raw material for Signify’s 3D-printed fixtures is ISCC PLUS certified and 71.5% renewable. Based on the colors and additives used in production alone, the officially mass-balanced rate will be “at least 55%”.
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.