Las Vegas, NV, USA, LDI Booth #3045 – Vari-Lite, the originators of the modern moving head light fixture and Signify (Euronext: LIGHT) entertainment lighting brand, is today announcing the VLHive 151 Digital FX, the world’s first all-digital entertainment lighting fixture. This next-generation luminaire, designed and manufactured at Vari-Lite’s Dallas, Texas, USA factory, includes a digital light engine, with 45,000 lumens of output and pixel-level control.
“While trendy new direct-view fixtures come and go every couple of years, core entertainment lighting fixtures have remained largely the same for decades,” says Martin Palmer, Vari-Lite Marketing and Product Management Leader at Signify. “LEDs have replaced lamps and additive color mixing has gained popularity, but the basic concept of shaping light using layered pieces of metal and glass remains. Because of this, there is a fundamental limitation to the looks possible in these fixtures because of the physical limitations inside the luminaire. VLHive is designed to change that.”
The VLHive’s 151-emitter LED array offers a variety of digital effects, including 360° rotating digital shutters, full-close digital iris, and a library of built-in digital gobos and multichromatic animations. Users can even create their own shapes and animations using the HiveCreator software tool. The VLHive 151’s exclusive, patented technology gives designers an endless range of unique effects, including effect smoothing, polar positioning, transition effects, and gobo keystoning—all of which can be controlled on the fly by standard DMX. And thanks to unique Vari*glass technology, designers can convert the large 12” front lens to a frosted projection surface at the press of a button, switching seamlessly from mid-air effects to direct-view animations on the fixture’s face.
Palmer explains, “The goal of VLHive is to foster better collaboration between lighting, video, and creative teams while remaining, at its heart, a light fixture. Video has seen a huge rise in production design in the past decade, and modern entertainment lighting needs to incorporate animated elements that align with these looks. At the same time, designers need to control and configure the fixtures dynamically using standard consoles and other lighting tools. In short, lighting designers need a fixture that allows them to work better with the rest of the design team, while retaining the qualities that make lighting unique amongst the rest of the stage design.”
The IP65-rated luminaire features an RGBL additive color mixing engine that provides a wide range of colors, from soft pastels to vibrant saturated hues. To improve the output and colors, the VLHive boasts exclusive technologies, such as SmartColor+ and FluxBoost®. SmartColor+ is an updated version of Vari-Lite’s color control solution for multichromatic engines that allows designers to select the perfect balance of output and CRI for their application while achieving the best-looking colors possible using familiar CMY color mixing control. And thanks to FluxBoost technology, designers get more output across the color spectrum, along with more saturation and more consistent light quality. This intelligent algorithm maximizes the output of enabled channels in multichromatic LED luminaires, for better power utilization and lumen output, whether you’re using a deep red or a cool white.
Sodhi continued, “The VLHive 151 opens a wide range of new opportunities for designers, aligning more closely with the rest of the production team for a more collaborative approach to the production design. Built with Vari-Lite’s commitment to longevity and featuring the widest range of design possibilities of any fixture on the market, the VLHive 151 promises to provide fresh design looks for years to come.”
Vari-Lite is showing the VLHive 151 Digital FX at LDI 2024 in booth 3045.
About Vari-Lite
Leveraging a rich legacy of innovation pioneering the entertainment industry’s most iconic lighting solutions, Vari-Lite offers an end-to-end portfolio of advanced, energy-efficient LED luminaires, data, architectural control, consoles, and power solutions that the world’s top lighting designers and consultants rely on to create unforgettable looks that amaze. This includes spectacular rock and roll shows, sporting events, moving dramatic performances, spiritual worship experiences, and memorable film and TV productions - at venues large and small.
Inventing the first modern moving head fixture for entertainment, Vari-Lite products have earned three Grammy awards, numerous patents and industry awards, and the devotion and respect of designers around the world. Our advanced, reliable, and intuitive solutions enable lighting designers to realize their creative vision.
Vari-Lite
S. Kyle Davis
Sr. Manager, Product Marketing and Communications
Tel: +1 817 233 2961
E-mail: kyle.davis@signify.com
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.
January 07, 2025
Philips Hue unveils AI-powered smart lighting and home security innovations
December 23, 2024
Signify included in Dow Jones Sustainability World Index for the eighth consecutive year
December 08, 2024
New digital Vari-Lite entertainment lighting fixture