Be the first! Get the latest news and updates
Suggestions

    How to take a BBQ to the next level

     

    August 24, 2022

     

    With the summer activities in full swing, why not create an ambient outdoor set up in your garden, to create the perfect environment for a BBQ with friends. Make sure the lighting is right so you can cook up a storm and enjoy the food with maximum pleasure. Philips Hue’s outdoor range can help you create the perfect set up for outdoor entertainment.

     

    Smart LED lights add an extra ‘oomph’ to events, no matter how casual. Your BBQ get-together becomes more special thanks to the simple addition of light enhancing the vicinity.

     

    Philips Hue lights can paint you garden in colour to add that extra touch to any event. Use the Hue app to set outdoor scenes for different situations. Set fun, bright scenes, such as Miami, to create the perfect ambience for your outdoor get-together and light up the garden with blue and pink.

    Add light to focal points

     

    A strip light is an easy, subtle way to add light to the focal points of your garden. The Philips Hue Outdoor lightstrip is ideal for direct and indirect lighting – it is easy to install, allows you to personalise your outdoor space and create a unique outdoor space. Place them along the edge of your patio to create a fun, surprising burst of colour — one of 16 million, to be exact — and help your space feel bigger. You can bend it, curve it, and light up pathways, highlighting features – making your outdoors yours. The Hue bridge is required for set up.

    Outdoor Lightstrip

    Illuminate your favourite spots

     

    The Lily Spotlight lets you highlight your favourite outdoor features, create interesting shadows and more. Simply connect the smart outdoor spotlights into any standard wall socket using the included low-voltage power supply to get millions of shades of white or coloured light in your garden. Illuminate your favourite elements of the garden with vibrant spotlights of colour. The Hue bridge is required for set up.

    Lily Spotlight

    Light up your walkways

     

    The Impress Outdoor Wall Light can be connected to your existing Hue bridge to enjoy all the features like away from home control and scheduling but is also great at creating ambience. Illuminate the walls to guide your guests into the garden with Impress. Compatible with Alexa, Google Assistant and Apple HomeKit. The Hue bridge is required for set up. 

    Impress Outdoor Wall Light

    Wash the walls with colour

     

    Wash large expanses of your outdoor spaces, such as fences, walls and hedges, with white and colour light. Part of the LowVolt system, the Amarant Linear outdoor light connects to a Philips Hue power supply unit and can even be connected to one another, creating a continuous wall of light. The built-in metal shield directs light upwards and out, creating an even spread of light across large surfaces – and eliminating harsh glare. This Philips Hue outdoor fixture is specially designed for use in outdoor environments and has undergone rigorous tests to ensure its performance. The Hue bridge is required for set up.

    Amarant Linear Outdoor light

    Take light with you wherever!

     

    Turn your personal space into all kinds of special by exploring endless combinations of soft light and colourful gradients. Bring the WiZ Mobile Portable Light along, anywhere inside or even outside your home and make your cosy corner truly inviting. It also has a dual-zone design that creates a beautiful gradient ombré colour effect with Dynamic Light Modes, allowing users to choose between two different light colours and creating an atmospheric ambience. This lamp features a touch panel for turning it on/off, and changing your favourite, pre-set light modes. A simple swipe will dim the light. You won’t even need your smartphone or a voice assistant.

    WiZ Mobile Portable Light

    With the temperatures reaching highs, take advantage of the outdoors and maximise your time outside with the assistance of light! Philips Hue and WiZ Connected can help you make these warm summer evenings better than ever, whether you want to relax or party, Hue and WiZ can help.

    About the author:

    Giuliano Ghidini

    Giuliano Ghidini

     

    Signify UK&I Consumer Commercial Leader

    For further information, please contact:

    Signify – UK&I PR Manager

    Nikita Mahajan

    Tel: + 44 (0)7459751618

    E-mail: nikita.mahajan@signify.com

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More blogs

    • Unlocking performance through lighting innovations

      December 17, 2024

      Unlocking performance through lighting innovations

    • Light at night that enhances our surroundings

      March 12, 2025

      Light at night that enhances our surroundings

    • Transforming Dubai’s iconic buildings with connected lighting from Signify

      December 17, 2024

      Transforming Dubai’s iconic buildings with connected lighting from Signify