Be the first! Get the latest news and updates
Suggestions

    Comber Greenway path is now lit

     

    February 10, 2024

     

    A popular walking and cycling path, the Comber greenway is a seven-mile-long traffic free route between Belfast and Comber. The route is used by pedestrians and cyclists for both commuting and leisure purposes. However, during the winter months and on dark evenings, the number of people using it was seen to decline. Here is how our lighting solutions helped increase footfall and make visitors feel safer on the path.

    Introduction

     

    A popular walking and cycling path, the Comber greenway is a seven-mile-long traffic free route between Belfast and Comber which has been enjoying increased footfall over the last few years.

     

    The route is used by pedestrians and cyclists for both commuting and leisure purposes. However, during the winter months and on dark evenings, the number of people using it was seen to decline.

     

    Following research by the Department for Infrastructure and consultation with local residents and users, there is now a LED lighting scheme under trial on the urban section of this traffic free route. This has improved visibility and the perception of safety for users after dark while minimising disruption to local wildlife and in particular the sensitive bat population. The lit-up pathway now is truly the vital community asset it was meant to be in East Belfast and can be enjoyed by residents who live along it and commuters who use it for walking and cycling right throughout the year. Read on to learn more about the project.

    Background

     

    The Department for Infrastructure in Northern Ireland has implemented a project to upgrade and illuminate a section of the Comber Greenway, a popular traffic-free route between Belfast and Comber. It is one of the most used urban greenways in Northern Ireland, and meanders seven miles out into the countryside along mostly flat terrain – making it popular amongst people of all abilities. The purpose of the project was to illuminate the walkway to allow pedestrians and cyclists to use it during the evening hours, especially in the winter months. The project now provides a safer space for those who wish to walk, wheel, or cycle all year round. What makes the project unique is the challenge it came with - obtaining lighting that would serve the public safely and protect the environment, as the area is known as a bat feeding corridor. The Department for Infrastructure, working with Signify, decided to install luminaires that have a special light recipe limiting the night time disturbance of bats whilst providing a light source with a colour rendering index (Ra) > 60 to promote safety and security for users.

     

    The design uses a special light recipe which has a high colour rendering, providing a safer feeling space for those who wish to walk, wheel or cycle all year round. The scheme has been designed with the local environment in mind. The design uses a light recipe which filters out the blue peak making the light source red in appearance. This spectrum has been proven to minimise the night time disturbance to bat colonies, while internal back louvres on the luminaires and lower mounting heights will minimise light spill into the hedgerows to shield wildlife and diminish light pollution into adjoining properties. 

    The technology in use

     

    The Department for Infrastructure working with Signify, who supplied LED lighting via their contractor M&P Bradley and promoted their Clearfield light recipe – this special light recipe has been proven to limit the night time disturbance of bats as the light source has no UV content and has removed most of the blue part of the spectrum. The spectral power is between 590nm and 790nm, giving the light source a red appearance with a correlated colour temperature (CCT) of 1000K.

     

    The project was installed by M&P Bradley early in 2023 and commissioned with Signify's CMS on 18th April 2023.

     

    The project uses 233 Philips Digistreet Micro luminaires connected with Interact Cellular Node, which allows for remote monitoring and control of the lighting system that brings lighting together with data and the IoT so you can create spaces that adapt to your needs, making them more efficient, connected, and sustainable.

     

    The project that is still in progress, will also see the installation of Multi Sensor radar detection installed in October. Multisensor is a Zhaga-D4i certified sensor connected to the luminaire via the Zhaga Book 18 socket and is the best choice for light on demand applications especially for cycling paths, as it has the capability to control a group of luminaires when motion is detected This allows the best use of light on demand by setting a low background level of illumination that can be increased when the radar is triggered by motion, providing a base level of illumination for the majority of the night to limit environmental impacts, whilst increasing the illumination level when required, providing a safer space for those who wish to walk, wheel or cycle all year round.

     

    The project was designed with the local environment in mind, using a special light recipe of the Philips ClearField technology which filters out the blue peak making the light source red in appearance, to limit the night time disturbance of bats, while internal back louvres on the luminaires and lower mounting heights minimised light spill into the hedgerows to shield wildlife and diminish light pollution into adjoining properties. Research undertaken shows some species of bat are light adverse and the introduction of lighting can have a negative effect on their commuting and foraging behaviours...

     

    Following consultation and engagement with residents, the new lights on the urban section of the greenway between Beersbridge Road and Billy Neill Halt have been programmed to operate during hours of darkness from dusk to 10.30pm and from 6.00am to dawn.

    Comber Greenway pathway lit with the Clearfield light recipe
    Comber Greenway pathway lit with the Clearfield light recipe

    The solution in action

    Comber Greenway leverages multiple technologies and innovations from the Signify portfolio. From ClearField, our biodiversity light recipe specifically developed in reducing the impact of light on bats – to our Philips outdoor luminaires with industry leading serviceability and one of the largest optical distribution options to suit any application – and our Philips Outdoor Multisensor with has been utilised in this project to deliver lighting on demand, right light at the right time – limiting light pollution and taking into account the ecology, whilst allowing the community to use this pathway in the darker months.’’

     

    Dervan Alleyne

    Director Public and Sports Lighting Solutions at Signify

    In conclusion

     

    The introduction of a new red spectrum lighting scheme, the first of its kind on these islands, is showing to make travel throughout the whole year more feasible while also minimising light pollution and protecting the local environment and bat population along this corridor. The pilot will be reviewed by the Department after two years and will help form a decision on whether the scheme should be further extended along the rural section between Billy Neill Halt and Comber. But there is no doubt that the project is already proving to be a win-win for citizens and the nocturnal animals in the corridor.

    About the author:

    Dervan Alleyne

    Dervan Alleyne

    Director Public and Sport Lighting Solutions Uk & Ireland · Signify

    For further information, please contact:

    Signify UK&I PR Manager

    Nikita Mahajan

    Tel: + 44 (0)7459751618

    E-mail: nikita.mahajan@signify.com

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More blogs

    • Unlocking performance through lighting innovations

      December 17, 2024

      Unlocking performance through lighting innovations

    • Light at night that enhances our surroundings

      March 12, 2025

      Light at night that enhances our surroundings

    • Transforming Dubai’s iconic buildings with connected lighting from Signify

      December 17, 2024

      Transforming Dubai’s iconic buildings with connected lighting from Signify