Be the first! Get the latest news and updates
Suggestions

    Optimal performance for demanding environments: Introducing the Philips PacificLED gen 5

     

    May 16th, 2022

     

    For industry and parking areas, a top-class lighting system that ticks all the right boxes is essential. With potential stresses, such as humidity, extreme temperatures, electrical sparks and chemical fumes, a robust solution is vital. 

     

    Lighting should also provide the right visibility at the right moment, to support the safe continuation of your operations. Then there are the financial considerations. It should be easy to install and maintain, offer an attractive total cost of ownership (TCO)., while harnessing energy efficiencies. All while meeting the greenest of environmental targets. Meet the 5th generation of PacificLED.

     

    The PacificLED gen5 is a solution that’s designed for optimal performance in the most demanding environments. With optional integration into Interact connected lighting system, enabling light management solutions, PacificLED can provide even greater energy savings, enhance safety and productivity. Making it future proof in every way.

    PacificLED Gen5
    Philips PacificLED gen 5

    Meant to light up in tough conditions

     

    PacificLED gen5 is suitable for a wide range of (heavy) industrial applications. The luminaires have a robust and compact product architecture, with high water and dust protection (IP66), combined with a high degree of mechanical protection (IK08). Designed for use in industry and parking areas, the luminaire can manage potential stresses like humidity, high temperatures, and chemical fumes to ensure industrial operations can be carried out in a safe manner.

     

    Industry: Due to its robust architecture, and compliance with industry regulations, PacificLED gen5 is the ideal choice for a plethora of industrial application areas such as warehouses and distribution centres, food processing and pharmaceutical manufacturing, discrete manufacturing, and chemicals and heavy industry. The luminaire is designed to withstand the worst that heavy industry can throw at it, from dust to oily vapours.

     

    Private and Public Parking: Excellent visibility is key; good light optimises driving conditions and gives people a feeling of safety and security. To avoid driver confusion and enhance safety; homogenous, high-quality lighting should be used to avoid lighting hotspots or striping. It should enable drivers to find a vacant space easily, park smoothly, and find the exit. But it should provide a bright space without creating disturbing effects or compromising operations or energy consumption. The Pacific gen5 meets this for under cover parking projects.

    Parking
    Philips PacificLED gen 5 - Parking Environment
    Manufacturing
    Philips PacificLED gen 5 - Manufacturing Environment

    Designed for the circular economy

     
    The PacificLED gen 5 is designed to meet the evolving needs beyond rated service life from start to finish – including service and repair, upgrades and replacements. The luminaire is designed around five principles of Signify’s Lighting for Circularity: recyclable, serviceable, energy-efficiency, connectable and upgradable, ensuring a long lifetime with high efficacy.

    Energy efficiency

     

    The PacificLED portfolio is proven to be highly energy-efficient, offering up to 160 lm/W as well as a long lifetime of up to 100,000 hours L80. Also, with integration to the Interact Industry system, the luminaire opens up additional opportunities for optimised efficiency, energy saving, connectivity, productivity and safety. This, combined with hassle-free installation and maintenance, ensures you enjoy an attractive TCO.

     

    ’The PacificLED gen5 is an innovative and best-in-class LED luminaire. We are excited to launch a lighting system that ticks all the right boxes and meets the demands and potential stresses like humidity, extreme temperatures and chemical fumes from industrial use and use in open spaces like under cover parking lots. In addition, the PacificLED gen5 is also designed with a circular approach, which means these are fully serviceable luminaires and can be upgraded to extend their overall lifecycle- making the luminaire future proof in every aspect.

     

    To make the PacificLED gen5 even more complete, the luminaire allows for integration with Interact, that opens additional opportunities for optimised efficiency, energy savings, improved light management, productivity, and safety – all while meeting the greenest of environmental targets.’’ – commented Nicky Hagan, Sales Manager Professional Trade, Signify UKI.

     

    If you are looking for a lighting solution to ensure a satisfied and productive workforce to minimise mistakes and increase production quality or if you are looking for a solution to enhance visibility in parking areas to aid safe driving and safety of pedestrians, the PacificLED gen5 can offer the right visibility. Create bright(?) spaces without disturbing effects, or compromising on operation, maintenance or energy consumption. PacificLED gen5 meets all the above.

     

    For more details visit Philips PacificLED gen5 | Philips lighting

    About the author:

    Ian Legg

    Ian Legg

     

    Product Marketing Manager, Signify UK&I

    For further information, please contact:

    Signify UK&I PR Manager

    Nikita Mahajan
    Tel: + 44 (0)7459751618
    Email: nikita.mahajan@signify.com

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More blogs

    • Unlocking performance through lighting innovations

      December 17, 2024

      Unlocking performance through lighting innovations

    • Light at night that enhances our surroundings

      March 12, 2025

      Light at night that enhances our surroundings

    • Transforming Dubai’s iconic buildings with connected lighting from Signify

      December 17, 2024

      Transforming Dubai’s iconic buildings with connected lighting from Signify