Be the first! Get the latest news and updates
Suggestions

    Philips lights up Notre-Dame as never seen before

    March 12, 2014

    Paris, France – Royal Philips (NYSE: PHG, AEX: PHIA), the global leader in lighting, today announced it is illuminating the interior of Notre-Dame de Paris with LEDs that will show off the cathedral’s gothic features as never seen before. Philips is placing LED technology at the service of 850 years of history, paying tribute to the architecture of this Gothic masterpiece. A total of more than 400 luminaires were used, with an installed capacity of just 30 kW, compared with almost 140 kW previously – reducing energy consumption by 80%.

    21st century technology to highlight a 13th century monument 
    With this new LED technology, the light appears to emanate from the stone, with the luminaires displaying the building while themselves remaining inconspicuous. Never dazzling, sometimes powerful, and always warm, this light creates a reverent atmosphere while still emphasizing the architecture.

    The lighting reveals the details of renowned works of art such as the Virgin and Child. This statue, which was moved to Notre-Dame in 1818, is the most famous of the thirty-seven representations of the Virgin that the cathedral contains.

    Today the profile spots redefine the characters while at the same time shining a gentle light onto the sculpture and the white flowers laid out at her feet.

    The north and south rose windows, which were made in the 13th century and symbolize the flowers of paradise, have also been highlighted.

    Positioned above the north and south doors, more than 50 meters from the rose windows, two completely invisible 250W spotlights direct their beams onto each rose window, revealing the delicacy of the sculptures. This lighting gives the impression that the stained-glass window itself is radiating light, without altering the monument’s exterior appearance, since the light is only visible on the inside.

    Lighting adapted to the Cathedral’s different activities “The Cathedral has two roles, a religious one and a cultural one, with religious ceremonies, visits (almost 14 million visitors in 2013) and concerts. The new lighting was therefore designed to allow different atmospheres to be created depending on these activities”, explains Armand Zadikian, the project’s lighting designer.

    Armand Zadikian was able to retain areas of half-light, to play upon the contrasts and to create effects of white tones. In order to integrate the lighting perfectly with the building and make the LED luminaires virtually invisible to visitors, he also worked in close collaboration with “Architectes des Bâtiments de France”, the official French architects’ body.

    Computerized orchestration 
    Specifically designed by Benoit Ferré, the resident bishop’s architect (European Architecture Company, EUROGIP), the major innovation of this project is the creation of a spinal column, horizontal, flexible and easily accessible. This technical column extends for three hundred meters, the length of the triforium.

    The 400 luminaires are operated by means of a computerized system, with a touch screen to simplify control. The system contains several lighting programs and Notre-Dame’s manager can add more if required.

    Almost all of the luminaires are dimmable, making it possible to modify the lighting according to the event taking place (ceremonies, concerts, prayers, etc.), the time of day or the season.

    Why was LED lighting chosen?
    The characteristics of LED lighting have several advantages:
    • Lower energy consumption: the 400 luminaires used have an installed capacity of just 30 kW, compared with almost 140 kW previously. The consumption of the lights in the nave, for example, has been reduced to a fifth of what it was.
    • A luminous efficacy far greater than that provided by conventional sources and instant ignition.
    • A longer lifespan of the installation: around 13 years for 10 hours of lighting a day (switching on and off does not affect the lamps’ lifespan).
    • A reduction in maintenance costs: LED luminaires require little maintenance. For example, the lights have LED flame lamps that reduce the number of maintenance-related operations (scaffolding and moving furniture), while at the same time cutting energy consumption by 80%.
    • Dynamic lighting that makes it possible to adjust the atmosphere of the site according to the religious or cultural activity (change of intensity and color).

     
    “Philips is very proud to have placed its know-how and technology at the service of this splendid project. For us the challenge was to devise effective lighting while respecting the authenticity of this monument, which attracts several million visitors every year. The lighting really had to enhance the beauty of the site without at any time overwhelming it”, says Benjamin Azoulay, General Manager of Philips Lighting France.

    The players in the project

    Project owner: Association Maurice de Sully
    Delegated project owner: Rector Monseigneur Patrick Jacquin
    Chief architect: Benjamin Mouton
    Main contractor: Benoît Ferré, architect of European Architecture Company EUROGIP
    Lighting designer: Armand Zadikian.

    For further information please contact:

    Aglaë de La Genardière

    Notre Dame de Paris
    Tel : +33 1 42 34 56 13
    Email: communication@notredamedeparis.fr

    Santa van der Laarse
    Philips Group Communications
    Tel: +31653400056
    Email: santa.van.der.laarse@signify.com 

    About Royal Philips

    Royal Philips (NYSE: PHG, AEX: PHIA) is a diversified health and well-being company, focused on improving people’s lives through meaningful innovation in the areas of Healthcare, Consumer Lifestyle and Lighting. Headquartered in the Netherlands, Philips posted 2013 sales of EUR 23.3 billion and employs approximately 115,000 employees with sales and services in more than 100 countries. The company is a leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as male shaving and grooming and oral healthcare. News from Philips is located at www.philips.com/newscenter.  .