Be the first! Get the latest news and updates
Suggestions

    Reporting at light speed as HSV becomes world’s first football club to use LiFi

    September 9, 2019

    Eindhoven, the Netherlands – Journalists in the press center at the Volkspark stadium - home to Hamburg football club HSV Fußball AG - are the first to file their stories using an innovative new means of wireless communication. This is because Signify (Euronext: LIGHT), the world leader in lighting, has installed LiFi in the stadium press center. The system, called Trulifi, provides journalists with a highly reliable, secure and fast Internet connection through the room’s ceiling lights. HSV is the first football club in the world to install the groundbreaking technology which uses light waves instead of radio waves to provide an Internet connection.

     

    New stadium of light

    The Volkspark stadium, which opened in 2000, has a capacity of 57,000 and is one of 10 stadiums that will host the European football tournament in Germany in 2024. It is also certified to host other top international tournament matches. Like many stadiums, the wireless signal in its busy press center was prone to overload due to journalists accessing the network and interference from mobile devices of fans, staff and officials, all pinging the wireless router.

    Journalists who write, edit and file stories under time pressure don’t want the added hassle of finding they can’t get online. Now the club is able to offer them a rock solid, secure and fast Internet connection along with high-quality, energy-efficient LED light that helps to lower the club’s carbon footprint.''

     

    Vierke

    Market Leader for Signify in the DACH region.

    Signify installed 84 Philips PowerBalance gen2 LED recessed luminaires in the stadium’s press center. Eight of the luminaires have an integrated Trulifi 6002 transceiver, which modulates infrared light waves to provide an Internet connection of up to 150 megabits per second (Mbps). Journalists using the system receive a USB Access Key, which plugs into their laptop. This picks up the LiFi signal and transmits data back to the luminaire. The LiFi system is free from interference and encrypted. Also, an extra layer of security is built-in as light waves cannot pass through walls.
     

    LiFi: World first for a football club

    “We opted for LiFi given the increasing demand for bandwidth from journalists using our press center. For them a reliable wireless connection is everything. Now they have good quality light to write their stories along with a reliable, fast and highly secure wireless connection,” said Daniel Nolte, segment leader area organization & infrastructure at HSV.
     

    Signify has a range of commercial Trulifi systems to satisfy different market segments. It also includes Trulifi 6013, which uses colored light to create a robust, secure fixed point-to-point connection with a speed up to 250 Mbps.
     

    Trulifi underlines Signify’s leadership in leveraging lighting infrastructure to unlock the potential of light in new high-growth segments with LED technology that’s not only innovative but energy efficient.

    For further information, please contact:

    Signify Corporate Communications

    Neil Pattie

    Tel: +31 6 15 08 48 17 

    E-mail: neil.pattie@signify.com

    Signify Corporate Communications

    Elco van Groningen

    Tel: +31 6 1086 5519
    E-mail: elco.van.groningen@signify.com

    Signify Media Relations DACH

    Stefan Zander
    Tel: +49 1607429087

    E-mail: stefan.zander@signify.com

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. With 2018 sales of EUR 6.4 billion, we have approximately 28,000 employees and are present in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been named Industry Leader in the Dow Jones Sustainability Index for two years in a row. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.

    Meydan Bridge

    More press releases

    • Signify's fourth quarter and full-year results 2024

      January 24, 2025

      Signify's fourth quarter and full-year results 2024

    • Pioneers of Light portal the platform to support all lighting applications

      January 21, 2025

      Pioneers of Light portal the platform to support all lighting applications

    • Philips Hue enhances immersive lighting experiences

      January 14, 2025

      Philips Hue enhances immersive lighting experiences