Be the first! Get the latest news and updates
Suggestions

    Signify takes circularity to the streets

    February 26, 2020

     
    • New generations of street luminaires Philips Luma and Philips Iridium are designed for a circular economy
    • Both generations of streetlights are easier to install and maintain
    • Can be connected to City Management Systems such as Interact City
       

    Eindhoven, the Netherlands – Signify (Euronext: LIGHT), the world leader in lighting, is launching two street luminaires that meet the requirements of a circular economy, are easy to install and maintain and can be connected to City Management Systems such as Interact City. Signify is developing products, systems and services for a circular economy to meet the increasing demand for sustainable technologies.

    Our current economic model of take-make-waste isn’t sustainable. I’m proud that with these two new streetlight generations we’re leading the lighting industry into this new economic model, which will allow us to extend the use of materials and avoid destroying resources and support our customers in implementing more sustainable technologies. Circularity will be one of the key customer requirements in taking decisions on streetlighting upgrades, in line with the growing attention to sustainable initiatives around the globe."

     

    Harsh Chitale

    Business Group Leader Professional at Signify

    According to a report by Northeast Group, there are approximately 308 million streetlights in the world, of which 27% are LED and only 5% connected.[1] Northeast’s expectation is that in the coming three years the number of streetlights will increase to 321 million, with the proportion of LED growing to 43% and connected lighting to 11%, illustrating the vast growth potential.
     

    The new generations of Luma and Iridium are fulfilling the requirements of a circular economy by being energy efficient in application, serviceable, connected, having a long/extendable lifetime and by being recyclable.
     

    Energy efficient in application

    Luma has an efficacy of 160 lumen/Watt and Iridium 155 lumen/Watt, making both best-in-class within their respective range. As components can be easily replaced, the luminaires can also be upgraded when future efficacy advancements are available. The luminaires can also be configured to best suit their application.
     

    Serviceable

    The introduction of GearFlex - a gear tray which includes driver, surge protector and other components - allows for opening and maintenance of the luminaires without the use of tools, which is a unique feature for both luminaires. This helps installers to replace and reprogram drivers within 30 seconds, without the need to touch any wiring and reducing the time they spend at a pole. This increases their safety and that of other road users. The luminaires also include a service tag that allows easy access to spare parts.

     

    Connected

    The luminaires are both system and sensor ready. They can, for instance, be connected to City Management Systems like Interact City, Signify’s wireless connected lighting system, turning street lighting into a connected network that can host sensors and other IoT-enabled devices. Interact City enables remote management of the streetlighting infrastructure, including the control and lifetime monitoring over the streetlights with just a few clicks, allowing operators to optimize operations, minimize energy consumptions, schedule preventive maintenance and to keep an overview of all the connected lights.

     

    Long/extendable lifetime

    Both luminaires have a lifetime of more than 100,000 hours. On top of that, spare parts and upgradeable components significantly prolong the product lifetime.

     

    Recyclable

    Luma and Iridium are designed to use natural resources in a much more effective and regenerative way. Most of the materials and components can be recovered for reuse or recycling, closing the materials loop according to circular economy principles.

     

    The Luma gen2 and Iridium gen4 luminaires will be available to Professional customers in Europe from March 2020.

     

    [1] Global Smart Street Lighting & Smart Cities Market Forecast 2019-2028 by Northeast Group

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. With 2019 sales of EUR 6.2 billion, we have approximately 32,000 employees and are present in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been named Industry Leader in the Dow Jones Sustainability Index for three years in a row. News from Signify is located at the Newsroom, Twitter, LinkedIn and Instagram. Information for investors can be found on the Investor Relations page.

    Meydan Bridge

    More press releases

    • Advancing lighting manufacturing excellence in India

      March 27, 2025

      Advancing lighting manufacturing excellence in India

    • Signify publishes 2024 Annual Report

      February 25, 2025

      Signify publishes 2024 Annual Report

    • Philips Hue Sync TV App Now Available on LG TVs

      February 25, 2025

      Philips Hue Sync TV App Now Available on LG TVs