Be the first! Get the latest news and updates
Suggestions

    New energy-efficient and durable Philips LED outdoor lights

    June 7, 2023

    New Philips LED outdoor lights combine energy efficiency and reliability in every season

    • New Philips LED lights for gardens and other outdoor spaces offer a durable and energy-efficient performance in the sun, snow and everything in-between
    • A-class LED outdoor lights include easy-to-install spotlights, posts, wall lights and pedestals with UltraEfficient Solar technology to reduce energy consumption and cost of living

    Guildford, UK – Signify (Euronext: LIGHT), the world leader in lighting, offers new energy-efficient Philips LED outdoor lights designed to perform in changing weather conditions while addressing the need to reduce energy consumption. The new spotlights, wall lights, pedestals, and spots for gardens and other outdoor spaces can withstand high temperatures and sun exposure, as well as heavy rain1. The lasting quality and brightness allow you to enjoy the outdoors year-round, while the LED lights and built-in UltraEfficient solar technologies help reduce energy consumption and cost of living 2

     

    Whether your garden is blanketed in snow or you are basking in the sun, to enjoy your outdoor space year-round, Philips LED outdoor lights are designed to perform in a wide variety of weather conditions. The solar lights maintain their brightness even during winter. Whether the season is gloomy or sunlit, the lights are built to withstand extreme temperatures as low as -20°C and as high as 40°C. They resist high sun and UV exposure as well as heavy rain and weather humidity up to 85%, without leading to corrosion or rust.1  

     

    Rising energy costs have influenced the cost of living. The new Philips LED outdoor lights include UltraEfficient LED or Solar technology to reduce energy consumption2,3. With a lifespan up to 50,000 hours2 they allow you to enjoy reliable and energy-efficient outdoor lighting in your garden, balcony, patio or driveway.

     

    Philips LED UltraEfficient Arbour wall lights, pedestals and posts provide warm white light for your outdoor space throughout the year, no matter the season. Compared to standard LED lights, they save 50% of energy due to their A-class LEDs2.

     

    Philips LED UltraEfficient Solar Tyla wall lights and pedestals are solar-powered and offer two levels of brightness that can automatically be activated by the built-in sensor. Enjoy the garden on a cosy summer evening with beautifully dimmed light, or let bright light help you navigate the darker days when entering or leaving the home. The power-reserve mode can be used so the lights only activate when motion is detected. The UltraEfficient Solar Tyla lights require no grid energy due to the built-in solar technology. With the right amount of light, they can last up to 500% longer3.

     

    Philips LED GardenLink Low Voltage system consists of spotlights, pedestals and accessories that offer bright light to illuminate your favorite outdoor spots and are designed to withstand the weather1. The simple plug-and-connect feature makes it easy to install the lights within a few seconds wherever needed. Additionally, the Dusk-to-Dawn sensor offers a timer control with four modes, which can be used to automatically switch the light on or off during certain times of the day.

     

    At Philips LED, we strive to meet the needs of consumers. Research has shown us weather resistance and durability are considered the key factors for outdoor lights. With changing weather patterns, we understand this is more important than ever.

    Philips LED outdoor lights stand out as they are designed and proven to perform in a wide variety of conditions. Additionally, the cost of living has gone up in the past year and outdoor spaces also offer opportunities for consumers to save energy - supporting the environment and the cost of living challenge.’’

     

    Michael Rombouts

    Business Unit Leader LED Lamps and Luminaires at Signify

    Availability

     

    • Philips LED Outdoor UltraEfficient Arbour (3000K, 3.8W, 800 lumen)
      • Wall light EUR 66.99, UK: GBP 64.99
      • Pedestal EUR 105.99, UK: GBP 99.99
      • Post EUR 132.99, UK: GBP 129.99

     

    • Philips LED Outdoor UltraEfficient Solar Tyla (3000/4000K, 0.2/1.2w, 55/255 lumen)
      • Wall light EUR 105.99, UK: GBP 89.99
      • Pedestal EUR 119.99 UK: GBP 99.99

     

    • Philips LED Outdoor GardenLink Low Voltage system (2700K, 6W, 600 lumen)4
      • Spot Black4
      • Utrecht Pedestal Anthracite4
      • Arbour Pedestal Anthracite4
    For more information about the new Philips LED outdoor lighting products, please visit www.lighting.philips.co.uk

    1Tests that have been performed: 1000hrs UV exposure with no yellowing or breakage; 500 hours of salt spray test and chemical solvate test to withstand corrosion and rust; extreme condition testing (85 degree with 85% humidity) for extreme weather condition withstand; waterproof testing at time 0 (out of factory) and after lifetime to ensure IP commitment during lifetime.

    2Comparing the Philips UltraEfficient luminaire with the Philips LED Bustan luminaire. The Philips UltraEfficient luminaire uses at least 50% less energy and offers 50,000hrs lifetime.  

    3Compared to the Philips Dusk Solar luminaire, the Philips Ultra Efficient Solar Tyla lasts 500% longer when the solar battery is fully charged.

    4Set up requires the separate UK compliant plug. Price and availability to be confirmed in Q4.

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More press releases

    • Signify's fourth quarter and full-year results 2024

      January 24, 2025

      Signify's fourth quarter and full-year results 2024

    • Pioneers of Light portal the platform to support all lighting applications

      January 21, 2025

      Pioneers of Light portal the platform to support all lighting applications

    • Philips Hue enhances immersive lighting experiences

      January 14, 2025

      Philips Hue enhances immersive lighting experiences