Keep an eye on your home with Philips Hue Secure cameras
Philips Hue Secure cameras feature a clear 1080p HD video feed with night vision to help you monitor your home in real time and trigger instant motion notifications. You can help deter intruders by triggering the unique combination of Philips Hue lights and sound alarms, or you can activate two-way talk to tell a delivery person to leave the package or just say “Hi!” to a friendly face. Philips Hue cameras feature end-to-end encryption by default, ensuring any video clips, snapshots, and live view remain private. Specifically, the capability to recognise whether a notification is triggered by a person, a pet or a package runs on the camera itself instead of the cloud, which means end-to-end encryption is always enabled.
Suitable for both indoors and outdoors, Philips Hue Secure cameras are available in both a battery and wired version, as well as in the colors black or white. The Secure wired camera can be used with a convenient desktop stand, giving you optimal flexibility to place it around the home. Both cameras can also be placed outside with the Secure camera mount with ground spike and can be easily connected to Philips Hue's existing low-voltage outdoor system.
Specifically developed for outdoor use, the Philips Hue Secure floodlight camera brings the best of the Philips Hue system together. It allows you to keep an eye on the backyard, patio, or driveway, and — when you trigger a light alarm from the Philips Hue app — the floodlight immediately illuminates a large area in any color, such as bright white or even red.
For all Philips Hue Secure cameras, a low-voltage outdoor charging cable and anti-drop cable are available.
Get alerted when doors and windows open with contact sensors
The Philips Hue Secure contact sensor — which can be used on doors, windows, cabinets, and more and is available in the colors black or white — sends real-time notifications when the contact sensor is opened or closed. For example, you can program your front door contact sensor to turn on your hallway lights and send a notification, so you can immediately check for potential intruders. You can also use the contact sensor to simply automate your lights anywhere else in the home: for example, you can program your lights to turn on and off when you open and close a cabinet or bathroom door.
All-new Security Center in the Philips Hue app
The Philips Hue app now features the new Security Center to control your smart home security system. When you receive a notification, you can tap it to open the app. From the Take action screen, you can manually trigger an alarm that flashes your lights, sound the siren on your Secure camera, or call the local authorities or a trusted contact.
Using the Philips Hue app, you can personalise your camera settings. Create Blackout zones, which make certain areas of the video feed private, or Activity zones, which prevent areas from sending notifications — particularly useful for busy sidewalks in front of the house. Users can arm and disarm the system, set up special armed states for whether they are home or away, review a timeline of events, and more.
Jasper Vervoort
Business Leader Philips Hue at Signify
How to access Philips Hue Secure
Philips Hue Secure starter kits and bundles conveniently combine a variety of products to start experiencing the new Philips Hue Secure system. The Philips Hue Bridge is required for the full suite of Philips Hue Secure products and their advanced features, such as the contact sensor, floodlight camera, light and sound alarms, automations, and more.
In order to ensure privacy and security of the Philips Hue smart home security system, it’s essential for users to have a Philips Hue account. Philips Hue accounts give users immediate access to their Philips Hue system and security features (even when they are away). Accounts also allow the administrators of a Philips Hue system to control individual member permissions in the app. Administrators can restrict members to only control the lighting, to control the lighting and arm/disarm the security system, or to have full control over the lights and security system.
Additional security features, which include access to Activity zones and detecting if a person, package, animal, or vehicle triggered the alert, can be unlocked with a paid plan. The Basic plan provides access to 30 days of video history, while the Plus plan offers 60 days of video history.
What else is new from Philips Hue
A new generation of the popular Philips Hue Festavia string lights will launch — and it can be used both indoors and outdoors. Besides creating a cosy indoor atmosphere for holidays and special occasions, any barbecue or backyard party can now be decorated with a gradient of colorful light. The new string lights come in three varieties: 100 LEDs along an 8-meter cord, 250 LEDs along a 20-meter cord, and 500 LEDs along a 40-meter cord. Three new light effects, specially made for Festavia, will be available in the Philips Hue app: Prism, Glisten, and Opal. These effects will also be available for first-generation Festavia string lights, while the Prism effect will be available for all Philips Hue color-capable lights.
The new Philips Hue MR16 smart bulb lets you bring Philips Hue smart lighting to conventional spotlights anywhere in the home. The bulb works on the same 12 V low voltage as standard MR16 bulbs, making them compatible with most transformers. Featuring a bi-pin base and standard width, these bulbs fit perfectly both in size and style into most existing fixtures.
Lastly, all Philips Hue users can benefit from the interoperability of Matter via a software update to the Philips Hue Bridge available in September 2023. With the launch of this update, users will see a simplified experience when connecting their Philips Hue system with other Matter-compatible smart home devices and apps.
Availability and Pricing
To find out more about the latest Philips Hue products and app features, visit www.philips-hue.com/newlaunches.
About Philips Hue
Philips Hue is the world leader in smart lighting. With its comprehensive range of products, Philips Hue brings smart lighting and security to everyday homes. Set the mood with beautiful colors and scenes, or even sync your lights to your TV, music, and games for a surround lighting experience. With Philips Hue Secure, you can help safeguard your home with cameras, sensors, and real-time notifications. Philips Hue gives you the opportunity to get the best light for any moment. For more information, please visit www.philips-hue.com. Stay up to date by following us on social media: Facebook, Instagram, Twitter, YouTube, Pinterest.
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.
January 21, 2025
Pioneers of Light portal the platform to support all lighting applications