WiZ lights that prevent, alert and deter – Signify launches a unique WiZ Home Monitoring proposition
Guildford, UK. Signify (Euronext: LIGHT), the world leader in lighting, is launching a unique Home Monitoring proposition to complement its WiZ smart lighting system that allows for the seamless integration of lighting and security in a simple, smart and secure way. WiZ continues to enhance your daily convenience with lights that simulate presence and trigger light alarms, a camera with night vision, and SpaceSense motion detection technology. By combining lighting and security, this new proposition helps consumers feel safe and comfortable in their homes.
Using the power of light and motion detection to deter intruders
WiZ unlocks Home Monitoring features in its smart lighting system, knowing that lights are already everywhere in your home and also one of the most effective ways to discourage potential intruders. With seamless user experience in mind, the WiZ app was optimized with intuitive features, such as customizable Monitoring Routines allowing you to both control your lighting and monitor your home with a single tap in the app. You simply need to click on your desired routine to let the WiZ system know you are going away and activate a set of lighting behaviors to help secure your home.
The WiZ app can now also notify you of unexpected activity in your home, allowing you to take immediate action. With SpaceSense motion detection technology, every compatible WiZ light is a motion sensor that detects every movement in the coverage area. The award-winning technology makes the WiZ smart ecosystem one of the most comprehensive and when combined with the new WiZ Indoor Camera, the system provides full coverage for your entire home. Consumers can activate WiZ monitoring for the entire home or only in certain areas and quickly turn it off when necessary.
To help you keep your home safe even when you are away, WiZ lights can be automated with presence simulation. They will turn on and off automatically pretending someone is home. You can decide how the lights will react when motion is detected: turn on to full brightness, flash, display vibrant colors, or something else.
Danny Lousberg,
Head of Software Product Management WiZ
WiZ Indoor Camera to keep an eye on your home
An important element of the new Home Monitoring proposition is the WiZ Indoor Camera, helping everyone create a secure environment at home. It allows you to control and see what’s happening in your home at all times, and will notify you of any suspicious movement or sound. As soon as you receive a notification, you can open the WiZ app to get a live view of what’s going on.
Being equipped with night vision, the WiZ Indoor Camera ensures that you can see everything at all times, even in the dark. Night vision is automatically enabled when the light level is low enough, using infrared to light up the space so you won't miss out on any details. The camera can also pick up on any sudden loud noises and send notifications when, for example, breaking windows or fire/smoke alarm noises are picked up.
A set of additional features make this camera ideal to secure your home, such as its two-way audio feature, image-based motion detection, wide 120 degree viewing angle, full HD, and an SD card slot.
WiZ will also provide an optional subscription service to unlock additional features like the possibility to store media from the WiZ Indoor Camera in the cloud for up to 30 days, define motion activity zones and/or privacy zones in selected areas or to start a manual recording while the WiZ camera is streaming.
How does that work in practice? Picture this – upon leaving on holiday, you turn on vacation mode and presence simulation at home, so that in case any movement is detected, your indoor and outdoor WiZ lights will flash, notifying neighbors of unwanted activity. The detected movement will trigger a notification on your phone, so you can immediately check the real-time view of your home within the WiZ app, as well as previously recorded media within the activity overview. And voilà! With WiZ’s home monitoring proposition you’re never in the dark, even when you’re not at home.
Availability
About WiZ Connected
WiZ Connected is an Internet of Things software solution provider focused on delivering easy-to-use, Wi-Fi-based smart lighting. Owned by Signify, the world leader in lighting, WiZ serves both consumer and professional markets in more than 70 countries. Learn more about WiZ Connected and how their innovative, connected lighting solutions make daily life easier at https://wizconnected.com.
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.
January 21, 2025
Pioneers of Light portal the platform to support all lighting applications