Be the first! Get the latest news and updates
Suggestions

    Architainment Lighting

    Meet the partner


    Architainment Lighting is a specialist project lighting company working in the architectural and entertainment sectors across the UK. We work with leading lighting designers, specifiers and architects to transform architectural, retail, and themed environments through lighting.

    Providing specifiers with the highest quality white light and RGB lighting fixtures and complete control solutions, Architainment Lighting offers clients a full service from conception, through specification to supply, integration, programming and system commissioning.
    Architainment Lighting logo

    Partnership level

    Gold Certified System Integrator

    Specialised in

    Building facades, airports, hospitality, retail, and interior down Lighting

    Projects

    The Foundation has  3 primary focus areas for project and partner selection:
    The Foundation has  3 primary focus areas for project and partner selection:

    London Eye
    London, United Kingdom


    Previously lit by fluorescent tubes that proved costly to maintain, and required manually installed gels to produce coloured light for special events. Architainment was approached to replace this archaic system with an LED-based alternative. Each fitting of ColorCast 14 can be individually programmed to generate millions of colours that are seamlessly produced by Chromacore technology, as opposed to the use of coloured gels. This technology gives the London Eye the cost-effective ability to display accurate colours for corporate clients and special occasions and is visible from more than a mile away.

     

    Find out more on the Color Kinetics website

    Green Wall at Snow Hill Station
    Birmingham, United Kingdom 


    The Green Wall at Birmingham, England’s Snow Hill Station is a mammoth structure that merges nature, architecture — and now, beautiful LED lighting. The impressive junction, which hides a multi-story parking lot and provides a scenic backdrop for the city’s future railroad network, measures 220 m x 7 m (720 ft x 23 ft) and showcases 604 m2 (almost 2000 ft2) of plants, making it the largest “living wall” in Europe. To add organic movement and vivid illumination to the living landmark Architainment specified the elegant white light LED fixtures from Color Kinetics. 

     

    Find out more on the Color Kinetics website

    Bluewater’s Winter Garden
    Kent, United Kingdom


    The aim of this project was to introduce a brand new lighting scheme to increase levels of daylight illumination at this retail and hospitality complex 25 miles east of central London. The highest-quality, energy-saving LEDs were specified and the result was a truly atmospheric and contemporary dining environment.

    • iColor Cove MX PC to illuminate circular cove detail
    • ColorBlast PC to light the glass ceiling
    • Visual clutter  reduced
    Architainment Lighting logo image
    A Signify and Architainment Lighting collaboration

    More about Certified System Integrators

    Become a partner