Eindhoven, the Netherlands – Royal Philips (NYSE: PHG, AEX: PHIA), the global leader in lighting, has launched Luminous Patterns, a programmable connected LED lighting system that can help architects and designers create a striking visual statement using a unique combination of light, patterns and materials. Philips Luminous Patterns are decorative panels, which consume little energy, are cost-effective and suited to a wide range of interiors, including bars, restaurants, retail stores, hotels and office lobbies.
Philips Luminous Patterns is a powerful new tool for architects and designers. It enables them to use light as an architectural material to create signature lighting design installations, from generating ambience with soft lighting to stimulating effects. Luminous Patterns is able to create a sparkling welcome in a hotel lobby, improve the atmosphere in a restaurant or reinforce a brand’s identity in a customer’s reception area.
“These embedded LED light patterns bring brilliance, warmth and sparkle into traditionally ‘mute’ architectural surfaces,” said Brad Koerner, Venture Manager Luminous Patterns at Philips Lighting. “Designers have until now felt that integrating lighting features in architectural surfaces have been difficult to specify, costly to manufacture, and risky to install. With Philips Luminous Patterns, designers can now embed innovative and eye-catching lighting features into their designs in a straightforward and cost-effective manner.”
The customizable light patterns are available in a broad range of lighting styles and textures that can be freely placed within custom-sized panels finished in a range of decorative coatings and in the graphic prints of choice. Also, customers are able to choose from four unique light effects: 3D Graphics, 2D Graphics, Round Sparkle, and Linear Sparkle. Production is based on a custom-order basis within the parameters of a standard configuration kit, enabling a simple and straightforward process from order to installation.
In addition, Luminous Patterns consume very little energy, with an entire installation using approximately the same amount of energy as a humble 60-watt bulb. Once installed, the innovative system is easily controlled via a digital control system. Each light point is controlled separately, meaning all of the points in a wall or ceiling can be programmed to create dynamic lighting effects.
Philips is bringing its global expertise and leadership in LED and connected lighting to transform the market for signature lighting design.
Notes to editors:
Philips is launching Luminous Patterns globally and it is available now. New light effects will soon be made available as well, and the pattern catalogue continues to grow.
Eeva Raaijmakers
Philips Lighting
Tel: +31 (0) 6123 505 97
Email: eeva.raaijmakers@signify.com
Royal Philips (NYSE: PHG, AEX: PHIA) is a diversified health and well-being company, focused on improving people’s lives through meaningful innovation in the areas of Healthcare, Consumer Lifestyle and Lighting. Headquartered in the Netherlands, Philips posted 2014 sales of EUR 21.4 billion and employs approximately 106,000 employees with sales and services in more than 100 countries. The company is a leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as male shaving and grooming and oral healthcare. News from Philips is located at www.philips.com/newscenter.
.