Be the first! Get the latest news and updates
Suggestions

    Philips Lighting casts a new light on North and South Block of Central Secretariat in New Delhi

    October 11, 2017

    Philips’ architectural LED lighting system offers a palette of 16 million colors to illuminate iconic government buildings

    New Delhi, India– Philips Lighting (Euronext: LIGHT), the world leader in lighting, today announced the illumination of North and South Block of the Central Secretariat building in New Delhi using Philips dynamic façade lighting. These iconic buildings house the Cabinet Secretariat, which administers the Government of India and are an integral part of India’s historical and political heritage.

    The buildings were built in 1931 and are home to the Prime Minister’s Office (PMO) and Ministries of Defence, Finance, Home Affairs and External Affairs of the Cabinet of India. Situated on Raisina Hill, New Delhi, the Secretariat comprises two blocks of symmetrical buildings (North Block and South Block) on opposite sides of the great axis of Rajpath, and flanking the Rashtrapati Bhavan, or the President's House.

     

     “We are honored to be involved in this prestigious project to illuminate the North and South Block of the Central Secretariat in New Delhi. Starting this week, our dynamic LED lighting will illuminate these buildings using a palette of 16 million colors that will accentuate the rich blend of traditional Indian and British architecture,” said Sumit Joshi, Vice Chairman and Managing Director, Philips Lighting India. “The new dynamic lighting system is also energy efficient and will make these buildings a visual treat.”

     

    Philips Color Kinetics utilizes the latest advancements in LED technology to create themes and customized light recipes that can be used for important national festivals and celebrations. Additionally, the system also has dimming features that will enable the buildings to reduce electrical consumption during non-peak hours. In all, approximately 662 light points have been implemented to create the stunning lighting effects. The light points are controlled by the advanced light management system, Philips Color Kinetics Light System Manager gen5, which can store multiple preset scenes, creating unique light shows with varied effects like ripple, cross-fade, particle and burst. The lighting was installed by the Central Public Works Department (CPWD), an attached organization of the Ministry of Housing and Urban Affairs, Government of India.

    For further press information, please contact:

    Philips Lighting South Asia

    Natasha Tandon

    Tel: +91 98 11 72 64 50

    Email: natasha.tandon@philips.com

    About Philips Lighting

    Philips Lighting (Euronext: LIGHT), the world leader in lighting products, systems and services, delivers innovations that unlock business value, providing rich user experiences that help improve lives. Serving professional and consumer markets, we lead the industry in leveraging the Internet of Things to transform homes, buildings and urban spaces. With 2016 sales of EUR 7.1 billion, we have approximately 34,000 employees in over 70 countries. News from Philips Lighting is located at the Newsroom, Twitter and LinkedIn. Information for investors can be found on the Investor Relations page.