Light Your World Blog
GoodLeaf Community Farms zero-touch vertical farm uses Philips LED production module to grow fresher, tastier, and more nutritious produce
Signify is bringing you the most complete stock offer in the industry with our new Ready to go portfolio that will replace Light to go in 2021
Signify is proud to be the only manufacturer who offers a comprehensive portfolio with both an extensive selection of lower wattage HID replacement lamps.
With 8 different styles in 2” and 3”, round and square, Lightolier has the largest array of cylinders in the US Market
With the HighFocus Gen 2 LED high mast luminaire we have added more lumen choices, more flexibility and lower pricing.
Later in 2020, Bodine will be releasing the Bodine BSL06M5, which introduces a novel way of installing the emergency LED driver with downlight fixtures.
The Philips FlexFit T8 LED Lamp was designed for most of your education, commercial and light industrial projects, keeping in mind convenience with flexible installation options.
Announcing the expansion of our MainsFit LED Tube product. MainsFit LED T8 retrofit lamp is a ballast bypass lamp so it eliminates the ballast which removes the need for future ballast replacement.