January 3, 2018
At Signify we continue to fulfill our promise to create forward-thinking, high-performance and aesthetically pleasing outdoor LED luminaires. We understand that the identity of a city and the needs of its residents are to be taken seriously.
#5 -RoadView LED roadway luminaire
The Lumec RoadView LED roadway luminaires were created to help those responsible for lighting our streets and highways succeed in their lighting design goals. Powered by the latest LED technology, and featuring innovative thermal management design, the RoadView offers exceptional performance and value. This versatile luminaire can be tailored to the unique specifications of each project by offering multiple LED boards and wattage options.
For more details, benefits and brochure: RoadView LED roadway luminaire
#4 -UrbanScape/MetroScape LED post-top luminaires
The Lumec UrbanScape and MetroScape LED post-top luminaires feature flexible, robust energy-saving solutions for heritage-styled urban architectural lighting. Crowned with an ornamental hood, the post-top model comes with a flat lens to highlight the thinness of the LEDs. These luminaires provide attractive lighting at night, adding appeal to the surroundings and promoting safe use of the environment.
For more details, benefits and brochures: UrbanScape and MetroScape LED luminaires
#3 -LytePro LED wall sconces (7, 16, 32 combined)
The low profile silhouette and compact appearance of Lightolier’s LytePro 7 LED wall sconces have high appeal across many building styles. Its low profile styling is ideally suited for use over doorways, garages, entranceways, wall signs or any applications where a lower mounting height and compact size is desired. LytePro 7 utilizes only 14 watts, and achieves up to 86 LPW to provide an efficient alternative to traditional light sources.
For more details, benefits and brochure: LytePro LED wall sconces
#2 -EcoForm LED site and area luminaire
In any outdoor site and area project, the next generation of Gardco EcoForm LED site and area luminaires are more than sources of illumination; they offer the best of all worlds: saving energy, saving time, and saving money for significant and enduring value. It’s not just about meeting technical requirements. It’s about looking out for the best interests of your customers, and going the extra mile to uncover new savings and conveniences!
For more details, benefits and brochure: EcoForm LED site and area luminaire
#1 -RoadFocus LED Cobra Head luminaire
With the new Lumec RoadFocus LED cobra head luminaires, you can now reliably upgrade to LED roadway lighting; saving energy, maintenance and operating costs, and contributing to environmental stewardship. At the same time, you’ll benefit from performance surpassing that of high intensity discharge (HID) luminaires while retaining the familiar cobra head design. In addition to enhanced light output with excellent uniformity, RoadFocus LED luminaires can help to drive cost and workflow efficiencies. Our luminaires are favorably priced, and also easily retrofit into existing infrastructures so you only purchase what you need, when you need it. With three sizes, a sleek, low-profile design, and many options, RoadFocus extends the same uniform aesthetic throughout all of your roadway applications. RoadFocus LED Luminaires are the only roadway lighting solution you will need.
For more details, benefits and brochure: RoadFocus LED cobra head luminaire
November 14, 2023
How lighting technology can help reduce risks to migrating birds