Dynamic LED lighting enhances the beauty and prominence of the cable-stayed bridge, Viaducto de la Novena in Colombia
Viaducto de la Novena, also known as Viaducto Provincial, is a cable-stayed bridge located in Bucaramanga, Colombia. The bridge stretches 550 m (1,804 ft) long and stands 130 m (427 ft) high, making it the longest urban bridge in South America and the tallest in Colombia. After overcoming underfunding issues and over four years of construction delays, the six-lane bridge was opened for traffic by the Bucaramanga Mayor Luis Francisco Bohorquez, Colombian President Juan Manuel Santos, Luis Fernando Arboleda, President of Findeter, a financial institution for development, and over 5,000 guests. To celebrate the long-anticipated opening, the mayor and the city's public lighting office decided the bridge needed lighting that would enhance the beauty and prominence of the Colombian landmark.
bridge lighting, bucaramanga, cable-stayed bridge, colombia, colorreach powercore, icolor accent mx powercore, led connected lighting, color kinetics, vaya linear mp rgb, viaducto de la novena, viaducto provincial
November 14, 2023
How lighting technology can help reduce risks to migrating birds