POP! is comprised of five Gumby-like creatures named POPO, POPUP, POPETTE, POPLI and POPOTIN who love to party. There are five mysterious luminous monoliths in the middle of Place des Festival, in which the five POP creatures are locked in. To free them, you will have to call them, coax them or even sing to them. With the public’s encouragement, the monoliths progressively light up and then the special creatures pop up and move to the music. They swing and sway bringing smiles and laughter to passersby and the public interacting with them. By simply gathering in front of them, the collective energy will awaken the POP family.