With SolarForm, you can expand lighting coverage to areas where conventional solutions are not possible. This aesthetically pleasing product can be quickly installed in areas without access to grid power, or where trenching is difficult. No area is too remote when the power comes from the sun!
When replacing traditional lighting, solar lighting solutions such as this can help you save money with reduced electric costs. You can also take advantage of government rebates and tax incentives. SolarForm, for example, qualifies for the federal Solar Investment Tax Credit (ITC), currently being offered by the U.S. Department of Energy. The ITC offers 26% for projects having commenced construction in 2020 (between January 1, 2020, and December 31, 2020), with a gradual decline to 22% in 2021, and 10% in 2022. Typically, solar lighting that is eligible for the ITC can also use an accelerated depreciation corporate tax deduction. To learn more about this government tax credit, please visit the U.S. Department of Energy’s Guide to the Federal Investment Tax Credit for Commercial Solar Photovoltaics.
Solar lighting is a key part of Signify’s commitment to sustainability, and we are excited to bring this environmentally-friendly solution to North America.
To learn more about the Gardco SolarForm, please contact your local Signify representative, or visit www.gardcolighting.com/solarform.
November 14, 2023
How lighting technology can help reduce risks to migrating birds