Signify is thrilled to announce the launch of the next generation of Lumec RoadFocus Plus luminaires! RoadFocus Plus is a full family of LED street lighting luminaires with an award-winning cobra head design and the ultimate in lighting flexibility. The launch of this innovative luminaire is another demonstration of our commitment to climate action, public safety and security, carbon neutrality, and connectivity – all areas where RoadFocus Plus shines.
RoadFocus Plus comes in four sizes, as well as multiple lumen packages and color temperatures. In addition, this roadway luminaire is available in a wide range of optical distributions ranging from 70 to 400W HID replacement and boasts industry leading efficacy of up to 200 lumens per watt. With the added high efficacy optics, you can achieve 36% more energy savings over the standard Roadfocus plus offering. This enhanced photometric performance in many cases will allow you to increase your pole spacing resulting in using less fixtures and savings on overall install costs.
Sustainability is at the heart of our business, and the RoadFocus Plus delivers a low carbon footprint impact on the environment. The family of luminaires are manufactured using less materials, resulting in a product that is an average of 30% smaller and 27% lighter than its predecessor. RoadFocus Plus is also packaged using 44% less materials than previous generations, which supports your goals towards carbon neutrality, a process we underwent, and achieved, as we have been 100% carbon neutral since 2020.
The exceptional features of RoadFocus Plus don’t end there. Ensuring that this product can not only meet your needs now but can support scaling in the future, RoadFocus Plus also comes with Service Tag, a QR-based identification system that provides installation, maintenance, and spare part information for the life of the product. These sophisticated connected lighting options come standard with a 7-pin receptacle and dimming driver and offers the Universal Zhaga Book 18 receptacle and D4i and SR drivers as options. This enables your RoadFocus Plus to be fully connectable now or in the future – you select the journey that works best for you.
November 14, 2023
How lighting technology can help reduce risks to migrating birds