BESbswy
BESbswy
Advance Express LED Drivers | Advance | Signify Lighting
You are now visiting the Signify website. A localized version is available for you.
Suggestions

    Replacing a LED driver has never been simpler

     

    Advance Express is more than just a product, it is a program to help you win in the replacement LED driver market.

     

    The Advance Express program offers a simple and fast solution for replacing drivers in existing indoor, outdoor, and downlight LED fixtures.

    Here's How It Works:

    • Locate the label(s) on the failed driver. It can provide all the information you will need to identify the replacement driver.
    • Order the replacement driver.
    • Read and configure the driver using the wireless programming tool or the MultiOne Mobile App.
    • Label the new driver with the programmed current to enable future maintenance.
    • Install the driver.
    Please review the material on how to determine a replacement driver. If you still have questions please contact us here:

    Recommended LED drivers

     

    Twelve recommended SKUs will replace an estimated 80% of commercial lighting driver applications. Additional SKUs to cover less common application such as 347V, 480V, and niche current/voltage combinations are also available.

     

    Contact us for full list of drivers offered in the Advance Express program.

    Getting Started

    Advance - Express drivers

    Determine the Replacement Driver

     

    Locate the labels on the failed driver. The two labels can provide all the information you will need to identify the replacement driver.

     

    See the training document below on how to read and collect information needed from the failed driver.

     

    Advance - Recommended process

    Order the Replacement Driver

     

    Recommended SKUs can be seen above, or contact us to see the full list and possible cross-references.

    Advance - Required accessories

    Program the Driver

     

    Read and configure the driver using these wireless programming tools:

    • MultiOne Express Software
    • MiltiOne Mobile Application
    • LCN9620 Programming Tool

     

     

    Advance - MultiOne Express Configuration System

    Label the Driver And Install

     

    No third-party software is required when printing labels via MultiOne Express.

     

    Label the new driver with the programmed current to enable future maintenance. MultiOne programming works with several third-party printers.

    Frequently Asked Questions

    How do I know that a driver has failed?

    The following signs could be indications that a driver has failed or reached the end of its useful life:

     

    1. The light output has noticeably dropped.
    2. The light is flickering or flashing.
    3. There is no light output and the wiring is correct & AC power is turned-on.  
    Are there standard drivers that work in most situations?
    Yes, the Advance Express program offers a list of commonly used drivers that  have a wide range of output current that can be configured to be suitable replacements  for exsisiting drivers. It is important when choosing a replacement driver that the power is appropriately selected and the form factor and application are matched. Please refer to  cross reference list located here.
    What information is needed to determine the correct replacement driver?

    To determine a replacement driver, you will need to gather the information below on the existing driver. Much of this information can be found on the label of the driver to be replaced. Here is the information you will need:

     

    1. The luminaire type (indoor, outdoor, industrial (high bay) or downlight)
    2. The mains power (should be on the driver label)
    3. The dimming interface
    4. Output current (check label)
    5. Output voltage of the driver (take highest number)
    6. If the existing driver is a class 2 driver or not
    7. Constant current or constant voltage
    8. Physical size of the driver that is being replaced
    9. If it is a downlight, is it a bottom entry or side entry connection?
    What information is needed to determine the replacement driver (cross reference) for an existing driver?

    To determine a replacement driver, you will need to gather the information below on the existing driver. Much of this information can be found on the label of the driver to be replaced.  Here is the information you will need:

     

    1. The luminaire type (indoor, outdoor, industrial (high bay) or downlight)
    2. The mains power (should be on the driver label)
    3. The dimming interface
    4. Output current (check label)
    5. Output voltage of the driver (take highest number)
    6. If the existing driver is a class 2 driver or not
    7. Constant current or constant voltage
    8. Physical size of the driver that is being replaced
    9. If it is a downlight, is it a bottom entry or side entry connection?
    There is no information on the driver. Where do you start?

    To get started in determining the replacement driver, please follow the steps below:

     

    1. Try to determine the type of luminaire it is: indoor, outdoor, industrial (high bay) or downlight
    2. Ask the customer to send a picture of the driver AND the label.  OR
    3. Go back to the original luminaire manufacturer and ask for replacement driver information for the specific luminaire.
    How do you read the label of a driver?
    Advance Express How To Read A Driver Label
    How do I read an Advance model number?
    Advance Express How To Read A Model Number

    When reading or ordering an Advance part number, please be sure to note the follow:

     

    • X0 vs. XO (should be the number “0” vs. the letter “O”).

    • XI vs X1 (should be the letter “I” vs. the number 1).

    • M suffix  refers to the driver being sold in multipacks. You can order a replacement driver with or without the “M” and it is compatible.

    What is a class P or class P listed driver?
    Any driver that is designated as "Class P" or "Class P listed" is allowed to be field-serviceable without the need to contact the original luminaire manufacturer, as long as the replacement driver is the same or lower power.
    What is the difference between a Class 2 and Non-Class 2 driver?

    When replacing a driver, it is important to know if the original driver is a class 2 or non-class 2 driver.

     

    • Class 2: Driver meets the limitations of < 100W and  < 60V and has gone through additional verification during the agency certification to conform to Class 2 requirements

    • Non-Class 2 (also sometimes referred to as Class 1): Class 1 drivers have higher wattage and/or higher voltage than class 2 drivers

     

    RULE: you must replace a class 2 driver with another class 2 driver.

    Can I replace a class 2 driver with a non-class 2 driver?
    This is not allowed per regulations.  A Class 2 driver must be replaced with another class 2 driver.
    Can I replace non-class 2 driver with a class 2 driver?
    Generally a non-Class 2 driver will exceed the power or voltage or current limitations of Class 2, so there will not be a matching Class 2 substitute. But, if a Class 2 driver is able to match the necessary power, current and voltage of the incumbent Non-Class 2 driver, it can be used as a replacement. 
    Are all class P drivers class 2?
    No, Non-Class 2 drivers can also be Class P.
    What does "Iout" mean?
    The letter "I" or current or "Iout"  is the symbol for output current.
    What is the difference between constant current and constant voltage?
    A driver is a constant current driver when it regulates the current directly for the specified range of LED voltage. Constant voltage drivers regulate a fixed voltage at the output, and the LED modules (or light engines) need to have additional on-board circuits to regulate the current in the LEDs.
    How do I know if I have constant current or constant voltage driver?

    To determine which type of driver you have, please refer to the list below:

     

    • The driver will typically state if it is constant current or voltage or will state CC or CV, either on the product label or the datasheet

    • If the driver specifies only one value for output voltage, it is a constant voltage driver (typically 24V or 12V). The LED module used with such a driver would usually call out this same voltage as an input specification, and usually also specifies a power rating. 

    • If the driver specifies a range of output voltage (and either a single value or a range of output current) then, it is a constant current driver.

    Generally most manufacturers indicate whether the driver is a Constant Current (CC) driver or a Constant Voltage (CV) driver on the product label or the datasheet. 

    What if a programmable driver is not labeled with the output current?

    It is important to replace a failed driver with a driver of equal or lesser output current.  To determine the output current:

     

    • If it is an Advance driver, the current can be read with MultiOne program and programming tool (LCN9620)

    • If it is not an Advance driver, contact the original luminaire manufacturer

    What are the various generations of products? Are they all replacements for each other?
    For Advance drivers, the trailing digit in the part number indicates the generation of the driver. Generally, a higher generation is a suitable replacement for a previous generation. When replacing a product belonging to the same generation (with the same exact part number) you can use MultiOne Mobile for Android phones and use the cloning function to "copy - paste" the settings from the source driver to the target driver. However, note that a newer generation cannot be cloned from a previous generation. You will need to read the settings from the source driver and then program the replacement driver using the  MultiOne Engineering PC based software.
    How many lamps can be put on one driver?
    This is a TLED question. Please refer to the cross-reference guide located here.
    What are the different types of dimming?

    Three most commonly used types of dimming are:

     

    1. 0-10V dimming

    2. Phase-cut (Leading Edge, Trailing Edge)

    3. DALI

    How do I know what type of dimming a fixture uses?

    Refer to the dimmer on the wall. Go to the website for the specific dimmer and determine what type of dimming it supports:

     

    1. 0-10V dimming

    2. Phase-cut (Leading Edge, Trailing Edge)

    3. TRIAC

    4. DALI

    5. D4i

    6. DMX

    Configuration tools

    MultiOne SimpleSet

    MultiOne Programming Tools

    MultiOne SimpleSet

    MultiOne Configuration Tool