It is important to replace a failed driver with a driver of equal or lesser output current. To determine the output current:
• If it is an Advance driver, the current can be read with MultiOne program and programming tool (LCN9620)
• If it is not an Advance driver, contact the original luminaire manufacturer