You are now visiting the Signify website. A localized version is available for you.
Suggestions
    Bodine - Emergency Lighting

    Bodine recognized twice in the 2020 IES progress report

    September 2020

    The Bodine GTDU and Bodine BSL06M5 recognized in the 2020 IES progress report


    Bodine is proud to announce that the Bodine GTDU and the Bodine BSL06M5 have been recognized in the 2020 IES Progress report. The IES Progress Committee accepts products based on their uniqueness, innovation, and significance to the lighting industry. Out of over 100 submittals, the GTDU and BSL06M5 are amongst two of the products recognized for their contribution to the lighting industry.

    The Bodine GTDU is an upgraded generator transfer device which features a dual Listing to UL 1008 (transfer switch) and UL 924 (bypass switch). It offers the smallest form factor for a UL 1008 device, 0-10V dimming control override, while reducing AC line current and power consumption.

     

    The Bodine BSL06M5 is our newest addition to the emergency LED driver family and is the first of its kind solution with a new compact design which helps provide a greater ease of installation by removing the need for conduits and additional emergency driver mounting normally found in standard LED emergency driver installations.

     

    The IES Report will be published in the November LD+A magazine and was presented at the virtual IES conference on August 30th, 2020.

    Bodine - GTDU and BSL06M5

    Highlights

    BSL06M5

     

    • New compact design for space-limited LED applications.
    • Plenum Rated Test Switch Cable Assembly
    • UL Listed for factory or field installation in the U.S. and Canada
    • Smart Charger Technology for low energy consumption
    • Meets Title 20 CEC (California Energy Commission) efficiency standards
    • Automatic code-compliant testing
    • Controlled power for predictable discharge
    • Color-coded, poke-in terminals to enhance wiring accuracy and ease of assembly/installation
    • Output Class 2 compliancy
    • RoHS Compliant

    GTDU

     

    • Dual listed to UL 1008 (transfer switch) and UL 924 (switch bypass)
    • 0-10V dimming control override capable
    • Reduced AC line current and power consumption
    • Universal input 120-277 VAC, 50/60 Hz
    • 24VDC fire alarm override capable
    • Allows ON/OFF switching of generator or central inverter supplied emergency lighting
    • Can be used with incandescent, fluorescent or LED lighting loads and provide full light output when in normal mode
    IES 2020 logo
    The GTDU and BSL06M5 are accepted into the 2020 IES Progress report.

    Downloads

    Coming soon BSL06M5

    More articles

    • The familiar and trusted, but better

      The familiar and trusted, but better

      The updated ELI-S-250 and the new extended runtime ELI-S-185 2-Hr are now available and make an exceptional lineup of emergency lighting inverters even better.

    • A new member for an already impressive product family

      A new member for an already impressive product family

      Bodine has added a new SKU to an already impressively large family. The BSL14B2 DF offers everything included with the BSL14B2 but with added flexibility in installation and mounting.

    • Small package, big deal

      Small package, big deal

      The small but mighty BSL10T3 and BSL06T3 are the smallest, most capable linear emergency LED drivers offered to date. Learn more about these unique products here.