You are now visiting the Signify website. A localized version is available for you.
Be the first! Get the latest news and updates
Suggestions

    What is LiFi?

    A paradigm shift

    Internet use is exploding. The global data communication volume is doubling every two years. This is caused by the number of connected devices multiplied by the data consumption of those devices.

     

    However, the radio spectrum does not provide enough room to grow. This manifests in reduced stability and less effective coverage of wireless connectivity as well as slower throughput, frustrating user needs and expectations.

     

    There is also growing concern about security with radio-communication. Radio provides a blanket cover, under which anyone could sneak. Unsecured or ‘open’ networks are an eavesdropper’s paradise.

    A paradigm shift

    What is LiFi?

    LiFi (short for light fidelity) is wireless communication technology which utilizes light to transmit data. It is a light communication system that is capable of transmitting data at high speeds over the visible light, ultraviolet, and infrared spectrums. In its present state, only LED lamps can be used for the transmission of visible light. In terms of its end use, the technology is similar to WiFi - the key technical difference being that WiFi uses radio frequency to transmit data.
    What is LiFi?

    Download the Trulifi brochure

    How Trulifi works?

    Simply put, Trulifi systems modulate light waves to transmit data using a transceiver. Then all you need is a USB access key, which can be plugged into your laptop to receive and send data. 

     

    Unlike other LiFi systems, it works whether the room lights are on, dimmed, or off. So it’s 24/7. Just like your business.

    How Trulifi works?

    The benefits of Trulifi

    • Designed to fit the application
    • Easy to install, commision, and use
    • Certified and industrialized
    • ITU standard protocol
    • Developed by the leading Lighting brand

    We'd love to hear from you