San Marcos, TX – The latest addition to the Philips portfolio of LED luminaires underscores the inherent flexibility of advanced LED design, and the latest in integrated technologies, such as built-in lighting controls and optics that meet exacting LEED light trespass requirements. In addition, PureForm from Philips Gardco features a modern aesthetic and state-of-the-art thermal management with the benefits of LED to deliver up to 65 percent more energy-efficiency over the pulse-start metal halide systems it was designed to replace.
Designed for use in parking lots, PureForm’s high performance optics allow for covering large areas with more uniform light quality and fewer pole locations, as well as offering a 4,000°K color temperature that rivals traditional metal halide systems. Delivering on the promise of LED, PureForm will also last significantly longer than traditional metal halide light sources.
The luminaire itself boasts a profile of less than three inches and a maximized lumen output range of 4,500 lumens to more than 25,000 lumens. Application flexibility is achieved via two different housing sizes and five distinct mountings, including three unique pole mount arms, a mast arm mount and wall mount versions.
As opposed to traditional systems that are either ‘on’ or ‘off’, PureForm offers intelligent controls such as integrated motion response and auto profile dimming. This allows for added energy savings by reducing the luminaire’s power consumption during off-peak hours.
Silvie Casanova,
Lighting Communications,
Philips Electronics North America
Ph: 781-418-7928
Email: silvie.casanova@signify.com
Royal Philips Electronics of the Netherlands (NYSE: PHG, AEX: PHI) is a diversified health and well-being company, focused on improving people’s lives through timely innovations. As a world leader in healthcare, lifestyle and lighting, Philips integrates technologies and design into people-centric solutions, based on fundamental customer insights and the brand promise of “sense and simplicity.” Headquartered in the Netherlands, Philips employs approximately 122,000 employees with sales and services in more than 100 countries worldwide. With sales of EUR 22.6 billion in 2011, the company is a market leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as lifestyle products for personal well-being and pleasure with strong leadership positions in male shaving and grooming, portable entertainment and oral healthcare. News from Philips is located at www.philips.com/newscenter.