Somerset, NJ – Philips Lighting has been honored with a total of seven Product Innovation Awards (PIA) from Architectural SSL Magazine. The award program recognizes the most innovative LED/solid-state luminaires and fixtures on the market, as well as the companies behind the components that make up these light sources. Products by Philips Lightolier, Philips Roadway Lighting, Philips Hadco and Philips Lumileds were recognized.
“Building on the success of last year’s inaugural program, our second edition of the awards proves lighting manufacturers are committed to solid-state lighting technology and are working arduously to deliver better performance, reliability and affordability,” says Jim Crockett, Editorial Director, Architectural SSL Magazine.
Lytespan products from Philips Lightolier received awards in the track lighting category. The Lytespan Mini LED Micro Cylinder is an exceptionally small 10-watt fixture with superior beam and glare control while the 15-watt
Lytespan Spot LED delivers powerful accent lighting using only 15 watts of power. The 15-watt Lytespan also received a special citation award for Standout Advancement in Technology, continuing a rich history of innovation in this category for Lightolier. Moreover, it garnered praise from one judge for being “a good-looking and excellent performing accent light that will make a great replacement for 50- to 75-watt halogen products. This is the best application for a track LED fixture I have seen; [it has] great overall simple design. It speaks softly, but carries a nice size stick.”
In the area lighting category, the new RoadView LED luminaire from Philips Roadway Lighting and the RX4 LEDGINE from Philips Hadco earned awards. The RoadView luminaire features an expandable design with anywhere from 32 to 160 LEDs, giving customers the ability to achieve the right light level for all applications. The RX4 LEDGINE is designed as an HID-replacement option in suburban street-lighting applications. Both outdoor luminaires benefit from the modular approach of the LEDGINE platform and best-of-breed Philips technologies such as Philips Xitanium drivers and LUXEON LEDs.
For a second year in a row, Philips Lumileds received awards for its LUXEON A and LUXEON S LEDs in the arrays/light sources category.LUXEON A LEDs are hot-tested and specified under real-world operating conditions, have a 85 degree C junction temperature, and deliver ”Freedom from Binning” initially with a 2,700K or 3,000K CCT. LUXEON S is a single LED package that rivals CDM and halogen solutions for spot applications in hospitality and retail lighting. Both LED solutions feature emitters with light output that falls within a single, three-step MacAdam ellipse centered on the black body curve.
“Philips continually pushes the boundaries of LED innovation and this latest series of awards demonstrates our commitment to providing customers with the best solutions for their application,” said Zia Eftekhar, CEO of Philips Lighting North America. “From the LEDs to fully integrated systems, we have one of the broadest, most advanced portfolios in the industry. With our modular approach, we help protect the LED technology investment and position customers for the future.”
The PIA winners were announced in Architectural SSL’s most recent e-newsletter and can be viewed online at
http://www.architecturalssl.com/sslinteractive/index.php?cid=5. The magazine will also host a press conference recognizing the products at LIGHTFAIR 2012 in Las Vegas this May.