Somerset, New Jersey – Signify (Euronext: LIGHT), the world leader in lighting, is launching the Philips UV-C disinfection box for small objects. The Philips UV-C disinfection box, fitted with Philips’ UV-C light sources, can inactivate SARS-CoV-2 (the virus that causes COVID-19 disease) on surfaces by more than 99% to below detectable levels1, providing an easy and effective way to disinfect items like keys, cell phones, toys and other household items.
Being at the forefront of professional UV-C innovations, Signify has applied its experience in UV-C lighting to develop the Philips UV-C disinfection box for consumers. It uses UV-C technology which has been proven by scientific studies to disinfect, in a couple of minutes2, against a vast host of viruses, bacteria, germs and mites3. Users can place multiple items in the box, close the lid, and their personal belongings will be disinfected. This will help to prevent the contraction or spread of viruses and germs when touching items.
Rowena Lee
Division Leader of Digital Products at Signify
Effective and safety-minded design
The Philips UV-C disinfection box contains a reflective stainless-steel interior designed to reach any surface of the object, whichever way they are facing. In laboratory tests, the Philips UV-C light sources with which the disinfection box is equipped, reduced SARS-CoV-2 (the virus that causes COVID-19) infectivity on surfaces by more than 99% to below detectable levels4.
As people and animals should not be exposed to UV-C light due to its harm to the eyes and skin, the built-in sensors automatically switch the device off when the cover is opened. This prevents any chance of UV-C light escaping and provides as an extra layer of protection for the user.
Functions and applications
With a width and height of 11 inches, the Philips UV-C disinfection box can be placed on any kitchen table or hallway table. The clear digital display offers an intuitive control with four functions. Besides the disinfect function, the storage function can continuously disinfect objects like toothbrushes or cutlery. Any moisture on personal items can be removed with the dry function. The disinfect+dry combination removes moisture and disinfects objects, like small toys and baby products.
Availability
The Philips UV-C disinfection box is available in the United States now, at selected retailers including Amazon, and via www.lighting.philips.com.
For more than 35 years, the company has been at the forefront of professional UV technology, building a track record of innovation in UV-C lighting. Signify is now leveraging this knowledge to address a growing need for the disinfection of surfaces, air and objects.
2 Disinfection effectiveness will vary depending on disinfection time, distance and type of surface/object. See product manual/webpage for details.
3 Malayeri et al., Fluence (UV Dose) Required to Achieve Incremental Log Inactivation of Bacteria, Protozoa, Viruses and Algae, 2016, accessible here.
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.
January 24, 2025
Signify proposes to re-appoint Gerard van de Aast to the Supervisory Board