You are now visiting the Signify website. A localized version is available for you.
Be the first! Get the latest news and updates
Suggestions

    Unleash colors from your TV screen with new WiZ HDMI Sync Box

    April 29, 2025

       

    Unleash colors from your TV screen with new WiZ HDMI Sync Box

     

    • WiZ announces the global launch of the HDMI Sync Box with TV Backlight, making it easier than ever to enjoy an immersive movie, sports watching, and gaming experience.
    • The HDMI Sync Box reads signals directly from video source and generates ultra-accurate color effects to make your lights match the on-screen colors in real time.
    • Elevate your TV experience by linking the new Gradient Light Bars and Gradient Floor light to the HDMI Sync box, creating wall washing effects in perfect sync with the TV.

     

    Eindhoven, the NetherlandsSignify (Euronext: LIGHT), the world leader in lighting, is unveiling new TV sync features and products for its smart lighting brand WiZ, enabling users to effortlessly immerse themselves in a world of dynamic colors and moods. With the new WiZ HDMI Sync Box with TV backlight, users now have an easy and affordable way to sync lights to their home entertainment content, taking their movie night, sports watching and gaming time to new levels. The new Gradient Light Bars and Gradient Floor Light are designed to be the perfect addition to your TV sync experience. After being configured in the WiZ app, they will match colors to the TV screen corresponding to their physical location and create a fascinating surround lighting experience.

       

    Bring your screen to life

     

    The WiZ HDMI sync box with TV backlight is all that the users need for bringing their screens to life. By simply connecting the Sync box to an HDMI media device such as a streaming stick, set-top box and gaming console, and attaching the LED strip to the back of their TV, users can make lights sync with the colors and brightness of the TV screen. No need to put a camera on top of your TV screen and there is no need for a complicated calibration procedure. It supports HDMI 2.0 and video formats up to 4K at 60Hz with HDR10+/Dolby Vision. The Sync box reads the video signal directly from the HDMI input, instantly analyzes the entire screen, and generates ultra-accurate colors on the lights. Featuring a three-side segmented RGBIC light strip for easy mounting on the back of TV, the HDMI sync box offers two different sizes, fitting TVs from 55” to 65” ($89.99) and from 75” to 85” ($109.99).

     

    The clean setup and personalized experience make the WiZ Sync Box perfect for every style and TV watching occasion. With the four preset sync modes – Cinematic, Vibrant, Relaxation and Rhythmic – and customizable brightness, color saturation and intensity, users can set lights to closely follow all the colors with drastic brightness change or to gradually transition while matching colors to the dominant hue on the screen. The HDMI Sync Box works with any WiZ color-capable light that supports both Wi-Fi and Bluetooth. Users can link as many lights to the Sync Box as they like (they need to be connected to the same Wi-Fi network) and make them sync with TV simultaneously. The Sync Box also has a built-in microphone that can capture audio playing from any source and make lights change colors and brightness with the music. Control is simple via the WiZ app, voice (with Google or Alexa) or the WiZ remote control. Users can also set the auto-switching feature in the app, so their TV sync lights will turn on and start syncing automatically whenever the HDMI media source provides a signal.

    At WiZ, we believe that enhancing your entertainment experience should be as fun and effortless as possible. Our new TV sync and vibrant smart lighting solutions allow users to transform any room into their personalized cinematic paradise. With intuitive controls and seamless integration, we empower everyone to enjoy the magic of smart lighting, making every viewing experience unforgettable.”

     

    Maikel Klomp

    Business Leader, WiZ Connected

       

    Compact design, remarkable ambiance: the Gradient Light Bars

     

    The Gradient Light Bars ($59.99) create captivating lighting in any space. Each light bar can be controlled individually and features a multicolor segment design that displays multiple colors simultaneously, creating beautiful wall-washing effects. Versatile in installation, the Gradient Light Bars come with various mounting brackets, allowing placement horizontally or vertically on counters or desks, or fixed behind TVs and monitors.

       

    Bring colors to any corner: the Gradient Floor Light

     

    The Gradient Floor light ($89.00) offers a multicolor segment design and wide beam angle, illuminating any room with stunning wall-washing effects. Its slim, minimalistic design fits effortlessly into any corner, complementing various interiors. It’s a one-piece design and features seamless plug-and-play functionality - no assembly required.

     

    Both the Gradient Light Bars and the Gradient Floor light deliver an engaging atmosphere by syncing colors with video (Sync box required) and with music. With 16 million colors and ready-to-use preset modes like Party, Fireplace and Ocean, users can set the perfect mood for any occasion. They are Matter compatible, so they can also be controlled with Alexa, Google Home and Apple HomeKit.

     

    The products will be available in May 2025. For more information, please visit www.wizconnected.com/explore-wiz/entertainment

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More press releases

    • WiZ launches HDMI Sync Box with TV Backlight

      April 29, 2025

      WiZ launches HDMI Sync Box with TV Backlight

    • Signify's first quarter results 2025

      April 25, 2025

      Signify's first quarter results 2025

    • Philips Hue Sync TV App Now Available on LG TVs

      February 25, 2025

      Philips Hue Sync TV App Now Available on LG TVs