New Philips T5 LED tube offers first true 1:1 replacement with widest ballast compatibility for 1500mm T5 fluorescent bulbs
Eindhoven, the Netherlands – Philips Lighting (Euronext Amsterdam ticker: LIGHT), a global leader in lighting, today announced the new Philips T5 LED tube to the Philips MASTER LEDtubes portfolio. The energy-saving T5 LED tube offers high light output and quality, and the widest ballast compatibility, so that it is a simple “click-to-fit”. The Philips T5 LED tube comes in a small form factor, providing a high performance of 150 lumens per watt.
Easy to fit installation and safety
Philips MASTER LEDtubes offer a 100% safe and easy installation with a simple lamp-for-lamp replacement. Using InstantFit technology, the T5 LED tube can fit straight into existing luminaires and requires no wire replacement. Electrically safe pins and the isolated driver make it easy to handle the tubes without the risk of shock. This will help installers to install quickly with precision, saving them time and money.
Long-lasting quality
The Philips T5 LED tube is made of polycarbonate to realize superior heat management over its lifetime. With a guaranteed lifetime of 50,000 hours the T5 LED tube outshines fluorescents with twice the lifetime and halves maintenance costs.
“While the average buying price of fluorescents might be less expensive, the total costs per year are more than double compared to Philips T5 LED tubes,” said Robert Boogaard, Product Manager at Philips Lighting. “To ensure further quality, we’re pleased to extend our warranty on professional LED lamps to five years. With the widest LED tube portfolio on the market, we’re able to ensure lasting light fit for every application whether car parks or offices, to schools and warehouses.”
The new Philips T5 LED tube is now available in most European markets and comes in the following types:
Philips Lighting, Global Media Relations
Bengi Silan Genc
Tel: +31 6 2544 1798
E-mail: bengi.genc@signify.com