What is included in the box?
• The RJ 12 cable to connect the Transceiver to the Access Point is included.
• The cable to connect the USB Key to a PC is included.
• The Plastic Optical Fiber (POF) cable to connect Access Points for synchronization in handover management is sold separately by Signify.
• The mains power cable for Controller is included in the unit packaging (EU or NA version).
What is not included?
• The RJ45 cables for the Access Points and the Controller are not included.
• The mains power cable for the Access Points is not included.