Be the first! Get the latest news and updates
Suggestions

    Orange Group’s Kirchberg store implements first LiFi installation in Luxembourg

    The Orange Group’s Kirchberg Shopping Center store is the first location in Luxembourg to install LiFi technology from Signify, known as Trulifi. The network was switched on in the presence of Eric Krier, Advisor in the Media and Communications Service of the Ministry of State.
    LiFi and 5G are two outstanding technologie
    LiFi, which stands for Light Fidelity, uses infrared light to send and receive information. While 5G has excellent performance outdoors, LiFi can take over indoors and deliver the high equivalent performance that Orange customers expect. “LiFi and 5G are two outstanding technologies that complement each other perfectly,” explains Mustapha Rahem, Distribution Director of Orange Luxembourg. “LiFi can transmit data to devices and make it possible to surf the Internet, send large files or collaborate online. Moreover, the two technologies can work in unison, as LiFi can be very easily connected to a Fiber Box or a 5G Box.”
    “We are proud to present this new connectivity technology in Luxembourg,” underlines Barbara Fangille, Head of Communication of Orange Luxembourg. “Already available for professionals since 2018, LiFi is also highly applicable for the general public. The sector is growing rapidly, and over time our current and future devices will naturally be compatible with this technology.”
    Trulifi from Signify lets users establish their own connection via a USB access key. It offers a high-speed connection, with up to 147 Mb/s download and 139 Mb/s upload, and a very low latency of less than 3 milliseconds. “To date, it is mainly the ultra-stability of this wireless connection as well as the absence of in interference with radio technologies that appeal to users,” adds Mustapha Rahem.
    USB access key

    “We are proud to present this new connectivity technology in Luxembourg. Already available for professionals since 2018, LiFi is also highly applicable for the general public. The sector is growing rapidly, and over time our current and future devices will naturally be compatible with this technology"

    Customer’s need

     

    An innovative technology (LiFi) that will grow to become a trusted alternative for wireless connectivity.

    Our solution

     

    Providing a wireless broadband connection, Trulifi by Signify uses infrared and visible light to enable high-speed, two-way wireless connectivity. The Trulifi solution can be integrated into luminaires or installed as separate ceiling units. With the LiFi Controller, seamless integration into existing network management dashboards is fast and easy. Customer-specific encryption gives an additional layer of security.

    The results

     

    Trulifi by Signify has been successfully installed in the new Orange store in the Kirchberg Shopping Center in Luxembourg.

    Customer

     

    Orange Communications Luxembourg S.A. is a fully converged telecommunications operator, which offers fixed and mobile telephony services, very high-speed mobile internet, fiber as well as cable or internet television for the professional and residential markets in Luxembourg. Orange Luxembourg S.A. is a 100% subsidiary of Orange Belgium, established in Belgium, and has been operating in the Luxembourg telecommunications market since May 2004. Signify and Orange are strategic members of the LCA based in Luxembourg.

    Download the Trulifi brochure

    Related Applications

    • Conference Center High Tech Campus Eindhoven

      Conference Center High Tech Campus Eindhoven

      Conference Center High Tech Campus hosts a variety of conferences and events. Having one of the conference rooms equipped with Trulifi was a natural thing to do.

    • Stirixis

      Stirixis

      Trulifi and Stirixis install LiFi at Pressious Arvanitidis in Maroussi, Greece for its fast, reliable, and secure wireless connectivity.

    • Globalworth installs Trulifi in Warsaw office

      Globalworth installs Trulifi in Warsaw office

      Globalworth chose the Signify solution not just because it is fast, but also because it offers the highest available level of security

    We’d love to help you keeping customer data safe