Be the first! Get the latest news and updates
Suggestions

        Transforming Dubai’s iconic buildings with connected lighting from Signify

     

     

     

    Scalable Philips Dynalite solutions go far beyond illumination

    While smart lights can be remotely controlled using apps, or automated to switch on and off at scheduled times, connected lighting systems use embedded sensors, two-way data exchange, and integration with third-party systems to transform environments and enhance people’s lives. 

    By collecting real-time data on building occupancy, temperature, and natural light levels, connected lighting systems can be continuously optimized to provide the best light in the most efficient way, reducing lighting-related energy consumption by up to 80%.”

    As a result, cities like Dubai are incorporating connected lighting into their most emblematic construction projects to support their sustainability objectives.

    Burj Khalifa: a towering achievement

     

    Standing over 828 meters tall, with 160 stories, the world’s tallest building is a marvel of engineering that required an equally impressive lighting control solution to bring it to life. 

     

    As well as the enormous façade, every private residence, office, and hotel room inside required a flexible lighting solution to meet its unique requirements. In response to this challenge, Signify developed a bespoke Philips Dynalite solution that sets new standards in scalability and functionality. 

     

    This state-of-the-art lighting control system is modular, with distributed control and monitoring to ensure consistent operation around the clock. Capable of time-dependent responses, the system is able to detect occupancy, time of day, and light levels to react and deliver the appropriate brightness and color temperature at all times. 

     

    The lighting control and automation system in each room is based on a common underlying architecture, with built-in intelligence and the appropriate levels of isolation right down to room level. 

     

    With 14,000 Philips Dynalite Revolution panels installed throughout the tower, the lighting in every room is individually controllable. Assembled in Australia from high-quality materials, the panels will maintain their sleek appearance and optimal functionality for many years, reducing the costs associated with routine maintenance. 

     

    In keeping with the building’s discreet luxury design, the entire system is also designed to be user-friendly and virtually invisible. Over 7,000 Philips Dynalite multipurpose controllers were installed in rack enclosures specially modified to be stored out of sight inside a utility cupboard.

    Atlantis The Royal: world-class lighting on demand

     

    Atlantis The Royal: world-class lighting on demand

     

    Like the Burj Khalifa, Dubai’s newest ultra-luxury hotel required a bespoke and scalable lighting solution. 

     

    Measuring 1.3 km across and 43 stories high, Atlantis The Royal needed a lighting system that could respond intuitively to occupant needs while maintaining its deluxe appeal throughout a variety of private businesses and common areas, including the iconic Skyblaze Fountain. 

     

    To help the resort shine in its best light, a highly advanced lighting control solution was designed and installed by two of Signify’s certified system integrators, Tectronics and BCL Dutco Tennant (BCL).

     

    The team mapped 452 DALI networks onto the DyNet control network, streamlining the entire venue’s lighting into a single cohesive system. The system can be monitored and controlled using System Manager, Dynalite’s multi-user management software tool.

     

    Due to its scalable network architecture and enhanced DALI capabilities, Philips Dynalite is perfectly equipped to light the enormous hotel. The Dynalite system is also integrated with third-party systems like air conditioning and blinds, allowing each area to transform at the touch of a button or through temperature, motion, and daylight sensing. 

     

    When the temperatures rise in summer, for example, the blinds lower automatically to block the sun’s glare and cool the room, while the blinds are kept open in winter to let the sunlight in.

     

    Illumination and beyond

     

    For both the Burj Khalifa and Atlantis The Royal, connected lighting systems have contributed to an environment of sophistication and luxury.

     

    The intelligent design of the Philips Dynalite lighting control system has made it possible to deliver functional and responsive lighting that is largely invisible to the end-user, with sophisticated automations and integrations powered by data to create an unforgettable experience for guests.

    About the author:

    Greg Nelson

    Greg Nelson

     

    EVP, Line of Business Systems and Services 

    For further information, please contact:

    Global PR Manager – Business Professional

    Krithika Bollamma B C

    Tel: +91 8123479307

    E-mail: Krithika.bollamma.b.c@signify.com

    For commercial enquiries:

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More blogs

    • Unlocking performance through lighting innovations

      December 17, 2024

      Unlocking performance through lighting innovations

    • Light at night that enhances our surroundings

      March 12, 2025

      Light at night that enhances our surroundings

    • Transforming Dubai’s iconic buildings with connected lighting from Signify

      December 17, 2024

      Transforming Dubai’s iconic buildings with connected lighting from Signify