Be the first! Get the latest news and updates
Suggestions

        Signify, DZE support performance and sustainability at Singapore GP

     

     

     

    Innovative lighting solution enhances the fan experience, consumes 30% less energy, and protects the night sky 

    Lighting the Marina Bay Street Circuit during night races is a complex task, with teams of engineers and technicians working tirelessly to ensure that everything is perfect. But the results are worth it: it’s one of the most hotly anticipated and visually thrilling races in the Formula 1 calendar, and a unique opportunity for Signify and DZ Engineering (DZE) to showcase their joint capabilities. 

     

    Preparation

     

    Given the temporary nature of the Singapore Grand Prix circuit, the lighting installation for the 5 km track needs to be set up from scratch every year. In order to arrange the infrastructure for over 1,600 floodlights and more than 220 km of cables in time for the race, DZE usually begins preparing the installation months in advance. 

     

    After a schedule is drawn up, a maintenance team conducts a thorough inventory check at a storage facility in Tampines. This ensures that all the necessary equipment from the previous race is still present and in working order. Installation typically starts in mid-June, with the first lighting tests taking place by the end of August, all in time for the Grand Prix which is usually held at the end of September. 

     

    Safety 

     

    Formula 1 cars can easily hit more than 300km/h. The Fédération Internationale de l'Automobile (FIA), the governing body of motor sports, created guidelines dictating that every track’s lighting system must create a safe environment for drivers and officials. Visibility is key, so the right illumination is absolutely essential, which provides the perfect stage for Signify to demonstrate its expertise.

     

    Assisted and supplied by Signify’s lighting experts, DZE installed over 1,600 Philips ArenaVision LED gen3.5 floodlights on trusses around the circuit, producing 75 times more light than a standard road lighting installation. In contrast to standard racetracks with permanent lighting systems installed at heights of 30 to 40 m, the Singapore Grand Prix uses a temporary installation on trusses at a height of 10 m, which do not interfere with the city skyline as would tall masts. The floodlights are positioned at strategic intervals along these trusses to ensure that the track receives bright, comfortable, and uniform light. The location, direction, and angle of each floodlight are also carefully adjusted to eliminate any shadows or glare that could affect drivers’ visibility.

     

    The race lighting system is designed to replicate the conditions of natural daylight, with a color temperature of 5700 K and an excellent color rendering score of 90. The right quantity, quality, and uniformity of light helps drivers to see the track clearly, without needing to wait for their eyes adapt to changes in brightness. In fact, given the incredibly high speeds at which drivers must react to their environment, the FIA considers uniformity of illumination to be more important than absolute illumination levels, as inconsistent lighting could hamper drivers’ ability to accurately judge their speed and distance from other cars, increasing the likelihood of accidents.

     

    Quality

     

    The right light is not only essential for the safety of the drivers, but it also adds to the aesthetic appeal of the race, creating a stunning visual experience for spectators, both those watching live at the track and via television all over the world.

     

    For televised events, consistency and quality of light are of utmost importance. Track lighting must be uniform and reliable so that broadcasters can capture high-quality images and video for audiences at home.

     

    Signify’s LED lighting system supports the latest TV broadcasting standards regarding glare and visible flicker. This allows broadcasters to perfectly capture the high-speed action against the backdrop of the city's unique skyline, ensuring that the view of the track can be enjoyed by Formula 1 fans everywhere.

    Philips ArenaVision gen3.5 LED floodlights reduced power consumption by 30%

     

    Efficiency

     

    Due to the growing importance of sustainability in the world of motor sports, the event’s race promoter Singapore GP Pte Ltd has announced plans to cut its energy emissions in half by 2028. Because night races depend on artificial lighting, this is one area where changes can be made to achieve incremental improvements in energy efficiency.

     

    The track’s lighting and control system, using floodlights and expertise provided by Signify and installed by DZE, is designed for maximum efficiency, with a guaranteed power supply to ensure safety and broadcasting continuity. Like lighting control systems for concerts and other entertainment venues, the Singapore Grand Prix lighting system is DMX capable. Although not currently in use at the track, this control system bridges the gap between functional lighting and show lighting, enabling technicians to create a unique and immersive experience.

    The Philips ArenaVision gen3.5 LED floodlights, which replaced the previous Philips system of conventional metal halide lights in 2023, has reduced power consumption at the Marina Bay Street Circuit by 30%. In addition, the use of highly directional light beams minimizes spill light, glare, and sky glow, reducing light pollution and minimizing negative effects on wildlife.”

    Philips ArenaVision LED gen3.5 floodlights on trusses around the circuit

     

    Success

     

    The lighting system supplied by Signify and installed by DZE at the Marina Bay Street Circuit represents a remarkable feat of teamwork between two experts in their respective industries. The 1,600 Philips ArenaVision gen3.5 LED floodlights installed on low trusses enable drivers to race safely at night, while also providing a thrilling spectacle for fans watching at the track and on television.

     

    About the author:

    Mark Gabbitas

    Mathieu Sergent

     

    Lighting Application Specialist

    For further information, please contact:

    For editorial enquiries:

    Tom Lodge
    Tel: +31 6 52525416
    Email: press.lighting@signify.com

    For commercial enquiries:

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. In 2023, we had sales of EUR 6.7 billion, approximately 32,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for seven consecutive years and have achieved the EcoVadis Platinum rating for four consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.

    Meydan Bridge

    More blogs

    • Unlocking performance through lighting innovations

      December 17, 2024

      Unlocking performance through lighting innovations

    • Light at night that enhances our surroundings

      March 12, 2025

      Light at night that enhances our surroundings

    • Transforming Dubai’s iconic buildings with connected lighting from Signify

      December 17, 2024

      Transforming Dubai’s iconic buildings with connected lighting from Signify