Signify is committed to the following medium-term guidance for the period 2021-2023:
• Yearly comparable sales growth of 0% to 5%
• Adj. EBITA margin of 11% to 13% in 2023
• Free cash flow above 8% of sales for the period 2021-2023
• ROCE of at least 11% for the period 2021-2023
Signify has 126,315 thousand ordinary shares outstanding and a free float of 98% (as per March 31, 2024).
The Dutch Financial Markets Supervision Act requires persons holding a capital and/or voting interest of 3% or more in Signify to disclose such to the Dutch Authority for the Financial Markets (AFM). The AFM processes these disclosures in its publicly available register, which can be found at www.afm.nl. An overview of the relevant holdings for Signify can be found here.
More information can be found here.
May 14, 2024 Annual General Meeting
July 1, 2024 Closed period Q2
July 26, 2024 Q2 & half-year results 2024 |