Be the first! Get the latest news and updates
Suggestions

    Sleek by design and connectable, new Philips SlimBlend luminaires invigorate offices, shops and hotels

    September 29, 2017

    • CBRE uses Philips SlimBlend in selected managed offices in Madrid to facilitate energy savings and employee wellness 
    • New Philips SlimBlend LED luminaires provide exceptional anti-glare and light quality

     

    Eindhoven, The Netherlands – Philips Lighting (Euronext: LIGHT), the world leader in lighting, today announced the availability of the new Philips SlimBlend LED luminaire, which meets the trend in offices and other commercial buildings for compact, energy-efficient lighting to suit high ceilings. CBRE Group, Inc. (NYSE: CBG), the commercial real estate services and investment company, is the first to install the new connect-ready LED luminaires, with its sleek and futureproof lighting design, in its managed office in Madrid.

     

    Vision for the working environment

    Philips SlimBlend LED luminaires will be installed over 1,000 sq. m over three floors at CBRE’s managed office in the Spanish capital. The office is located in Paseo de la Castellana, commonly known as La Castellana, one of the longest and widest avenues of Madrid. The installation meets the firm’s objective to have the best working environment for its employees. Philips SlimBlend’s aesthetic design and its high-quality light output supports the company’s vision for staff wellness with the ability for light to be aligned to daylight patterns.

     

    Mariano García, head of Design and Build, Building Consultancy at CBRE Spain said, “The market for office space is highly-competitive. By moving to the new Philips SlimBlend LED luminaire family we are leading by example to enhance our employees’ working environment so that the offices we manage are consistently lighter, brighter and more pleasurable. In addition, LED technology presents us with up to 50% energy savings when compared to conventional lighting.” 

     

    Annual energy consumption in offices and buildings

    Philips Lighting estimates that on average, lighting consumes around 25% of the annual electricity consumption of offices and buildings. Philips SlimBlend’s LED technology can reduce electricity used for lighting by up to 50% in comparison to conventional lighting. 

     

    Philips SlimBlend LED luminaires are connect-ready and can be recessed, suspended or surface-mounted and provide a typical energy saving return on investment (ROI) within three years. Featuring Philips Lighting’s Micro Optics technology, the Philips SlimBlend family of luminaires reduce light from angles between 65° and 90°. Aside from reducing glare, the luminaire family has the benefit of a large surface light area and a high-end look.

     

    “We are able to deliver an exceptional quality of light with the new Philips SlimBlend luminaire family which uses our patented Micro Optics technology to reduce glare and increase comfort for employees. The new range is an integral part of our strategy to provide end-to-end lighting systems and services for offices, retail and hospitality sectors. In addition, the luminaires, equipped with built-in sensors for applications such as room occupancy and motion detection, provide a solid foundation for both existing and future connected lighting systems,” said Paul Peeters, Business Leader Professional Lighting Europe at Philips Lighting. 

     

    Notes to editors:

    • Philips SlimBlend LED luminaire family has a lifetime of 50,000 hours, which is three times longer than conventional lighting. It has a luminous flux of 2,800, 3600 and 4200 lumen and a correlated color temperature of 3000K and 4000K.
    • The Philips SlimBlend LED luminaire family is available now in Europe and is suited to retail, hospitality and new offices using the Philips Power over Ethernet (PoE) and Philips SpaceWise systems as well as retrofitting existing offices, integrating with the Philips InterAct Office system.

    For further information, please contact:

    Anne-Marie Sleurink

    Philips Lighting Media Relations

    Tel: +31 6 22 30 65 29

    Email: anne-marie.sleurink@signify.com

    About Philips Lighting

    Philips Lighting (Euronext: LIGHT), the world leader in lighting products, systems and services, delivers innovations that unlock business value, providing rich user experiences that help improve lives. Serving professional and consumer markets, we lead the industry in leveraging the Internet of Things to transform homes, buildings and urban spaces. With 2016 sales of EUR 7.1 billion, we have approximately 34,000 employees in over 70 countries. News from Philips Lighting is located at the Newsroom, Twitter and LinkedIn. Information for investors can be found on the Investor Relations page.