Eindhoven, NL - Signify (Euronext: LIGHT), the world leader in lighting, has announced new smart light products, including an upgraded Hue Go, the Smart button, the Smart plug, and new GU10 and E14 smart bulbs.
The Hue Go portable smart lamp: bring smart light anywhere
The Philips Hue Go is a portable smart lamp offering colored smart light, including preset light recipes and scenes — and it now features Bluetooth capability, meaning you can control it with the free Hue Bluetooth app or your voice via selected smart home assistants. Retaining its signature design, the upgraded Hue Go also features an improved battery life, meaning you can now bring it with you anywhere you like for an even longer period of time.
Smart plug and Smart button: small size, big impact
The Smart plug turns any table or floor lamp — even those in which you can’t place a Hue bulb — into a Hue smart light. Simply connect any lamp to the Smart plug and add it to your Philips Hue setup, switching it on or off as you would control any other light using the Philips Hue Bluetooth app, a smart accessory, or your voice.
The Smart button, though subtle in size, packs a big punch — in a single press, you can control your Hue lights however you like, or press and hold the button to brighten and dim. When connected to the Philips Hue bridge, you can configure it so it turns your lights to a preset white shade and brightness adapted to the time of day: in the morning, one touch will turn your lights to cool tones and in the evening on touch will trigger warmer light settings. With a magnetic back side and its adhesive mini mount, you can place it wherever you need it. It also includes a larger backplate with the same dimension as your standard single gang wall switch, making it a smart replacement for your existing wall switch!
New build-on and recessed spot lights: add a touch of modern
Add a touch of contemporary elegance to any room with the Philips Hue White and color ambiance Fugato and Argenta build-on spot lights, available in single, double, triple, or quadruple-light fixtures. For a subtler look, use the new Philips Hue White and color ambiance Centura recessed spot light in either the round or square version. Both series of spot lights are Bluetooth enabled which makes setting the perfect scene just a simple click away.
GU10 spot lights: a new generation
New Bluetooth-enabled White and color ambiance GU10 spots give your built-in and recessed spot lights a burst of color and add style to any room of your home. This new bulb features exciting upgrades: higher lumen, richer color and a new design that now perfectly fits in your spots ! Rather than relying on a single switch to turn on or off all your spot lights at once, you can control these bulbs individually in the Hue app.
E14 candle bulbs: light up your space in style
The new White E14 candle bulb give you more choice when selecting your home lighting. Ready to use after a simple setup with Bluetooth or a Hue Bridge, these bulbs are the perfect addition to the Philips Hue range.
The Adore bathroom range: bathe in perfect light
Philips Hue has expanded the Adore range to include more lights for the bathroom, including a recessed spot and a large and small version of a slender, horizontal mirror light. The recessed spots pack, which features three spots, and each of the two mirror lights include a Hue Dimmer switch for easy control. Featuring four default light recipes, the Adore range provides the best light — cool to warm white — to make your daily routines, such as applying makeup in the morning or soaking in a relaxing bath at the end of the day, that much easier.
Pricing and availability
For more information about the new Philips Hue Filament collection, visit www.philips-hue.com.
Signify (Euronext: LIGHT) is the world leader in lighting for professionals and consumers and lighting for the Internet of Things. Our Philips products, Interact connected lighting systems and data-enabled services, deliver business value and transform life in homes, buildings and public spaces. With 2018 sales of EUR 6.4 billion, we have approximately 28,000 employees and are present in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been named Industry Leader in the Dow Jones Sustainability Index for two years in a row. News from Signify is located at the Newsroom, Twitter and LinkedIn. Information for investors can be found on the Investor Relations page.
Philips Hue is the world’s leading connected lighting system for the home. It comprises bulbs, strips, spots, lamps and controls. The system is transforming how light is used in and around the home to stimulate people’s senses, light their moments and help provide peace of mind when away from home. Through a vibrant developer program there are more than 750 third-party apps for Philips Hue.
For more information, please visit www.philips-hue.com. Follow us on our Social channels to stay updated: Facebook, Instagram, Twitter, YouTube, Pinterest
April 25, 2025
Signify delivers update on CEO succession process; CFO Željko Kosanović appointed interim CEO