Eindhoven, the Netherlands – Signify (Euronext: LIGHT), the world leader in lighting, will help customers manage their energy expenditure with a new range of Ultra Efficient lights and, for the first time, Ultra Efficient integrated luminaires. The new, more diverse product range offers customers even more opportunities to integrate the most efficient energy-saving LED lighting into their homes.
The new lights and luminaires join the Ultra Efficient A-class Philips LED bulb, which was the first light bulb to meet the new A-class standard in Europe in 2021. At a time of raised public awareness of energy costs, these lights consume at least 50% less energy and last 50,000 hours, which is much longer than standard Philips LED lights. All Ultra Efficient products are designed to achieve an A-class rating under the new, stringent European energy labeling that was introduced in 2021.
Saving energy with Ultra Efficient lights and luminaires
Lighting accounts for a substantial amount of household energy use, and consumers can expect to see a significant increase in energy bills as winter approaches. Changing conventional lights or LEDs to extremely efficient LED alternatives can have a powerful impact on reducing energy consumption.
Depending on their current light usage, households could save up to €34 per light, per year just by replacing incandescent lights with Ultra Efficient lights. This equates to a cost savings of €347 per year for just 10 lights. Over the lifetime of the product, they can enjoy savings of over €14,000.2
In addition, the products’ high level of energy efficiency and long lifetime dramatically reduce both consumer waste and carbon emissions. There are 1.7 billion conventional light points in homes across the European Union that have not yet been upgraded to LED. If all these lights were changed to Ultra Efficient LEDs, carbon emissions could potentially be reduced by 10.7 million tons per year. This is equivalent to the CO2 sequestered by 487 million trees annually.3
Meet the Ultra Efficient luminaire range from Philips
The new Philips Ultra Efficient luminaires are designed to meet the most stringent EU Ecodesign and Energy labeling regulations, with an A-class light source included, and efficacy up to 210 lm/w. These Ultra Efficient luminaires consume at least 50% less energy and last 50,000 hours while beautifully lighting up homes. The highly energy-efficient luminaires, available in various lumen packages and product categories, offer significant cost savings as energy prices rise.
With the Philips Ultra Efficient indoor range of downlights, customers can enjoy ultimate energy savings combined with a clean, aesthetic design. The new indoor luminaires—which meet stringent Philips EyeComfort4 criteria—are the brand’s most energy-efficient indoor lights yet.
The Philips Ultra Efficient outdoor range includes both a wall light and a pedestal light. Both are made from durable material and designed to perform in all weather conditions. The solar luminaire range has also been upgraded with superior technology for ultimate energy savings. Because of their longer-than-ever lifetime, all Ultra Efficient luminaires come with a 5-year warranty.5
Availability
Consumers will recognize the new, expanded line of Philips Ultra Efficient LED lights and luminaires by the same zero-plastic packaging and design that other Philips products use, but now with a green background color, illustrating the company’s commitment to providing global consumers with sustainable lighting products. The new products will be available starting October 28, 2022.
Products
Indoor luminaires
Outdoor luminaires
Lamps
1 In comparison to standard Philips LED products. Standard Philips LED products Meson downlights, Bustan wall lights and pedestal lights, and Dusk wall lights and pedestal lights.
2 Energy savings are calculated based on www.overstappen.nl (reference date May 2022, Dutch energy tariff for households) in comparison between a 2W Ultra Efficient LED integrated downlight versus a conventional downlight with an incandescent 40 W bulb at 4 hrs/day usage. The calculation is based on savings of 34.7 per light per year x 10 lights x 50000 hrs lifetime ÷ 1200 hrs per year usage, on Dutch energy prices. Actual savings will differ based on local energy prices. http://appsso.eurostat.ec.europa.eu/nui/show.do?dataset=nrg_pc_204&lang=en
3 The average wattage for all types of incandescent lamps is 60 W (approximately 700 lumens). The average wattage for all types of halogen lamps is 50 W (approximately 700 lumens). The average wattage for all types of CFLI is 14 W (approximately 810 lumens). http://appsso.eurostat.ec.europa.eu/nui/show.do?dataset=nrg_pc_204&lang=en
4 Designed for the comfort of your eyes. Visit www.philips.com/eyecomfort for flicker, strobe and other criteria and product details.
5 Refer to Philips Home Luminaires Warranty Conditions - For Europe
Signify Corporate Communications
Abigail Levene
Tel: +31 6 2939 3895
E-mail: abigail.levene@signify.com
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.
April 16, 2025
Signify completes share repurchases to cover share-based remuneration and continues with the share repurchases for capital reduction