Be the first! Get the latest news and updates
Suggestions

    Signify’s Trulifi brings connectivity to pioneering Berlin school

    November 7, 2022

    Signify’s Trulifi technology brings best-in-class connectivity to pioneering Berlin school

     

    • Berlin's Freie Waldorfschule enjoys high-performance, secure data connectivity through light waves
    • Nine rooms are equipped with custom-built transceivers and USB access keys
    • The school joins a growing number of educational facilities adopting Trulifi worldwide

    Eindhoven, the NetherlandsSignify (Euronext: LIGHT), the world leader in lighting, has equipped a Berlin school with Trulifi technology to enable fast, secure data transmission through light waves. Students and teachers at the Freie Waldorfschule in the Prenzlauer Berg district can now enjoy high-speed access to a wide range of online learning resources, independent of a WiFi connection. With this initiative, the school joins educational institutions in Italy, Germany, Belgium, The Netherlands and the US that are already using Trulifi by Signify.

     

    A secure and reliable Internet connection is not only crucial at work; the education sector also relies increasingly on the benefits of modern connectivity. Signify's Trulifi technology is a dependable alternative to regular Wi-Fi in locations where radio frequencies are not allowed or restricted, or could cause interference, as is often the case in schools. The technology guarantees high transmission rates, which are independent of the radio frequency spectrum and do not suffer from overloads caused by too many devices on the same frequency. The use of USB access keys secures access only to authorized people and devices.

    Fast and secure Internet via USB Access Key

    Working closely with Signify, the Freie Waldorfschule opted to equip seven classrooms, a conference room, and a science lab with the Trulifi 6002 system. With down and upload speeds of 220 Mbps, the technology provides enough capacity to meet the data needs of all the students in a classroom.

     

    A total of 114 specially designed ceiling-mounted transceivers were installed, laying the foundation for data transmission through light. Since July, the school has been running a test phase to connect the school’s notebooks with the transceivers. As soon as the access key is plugged in, a connection is automatically established – regardless of whether the lighting is on, dimmed, or off. This is one of Trulifi’s unique selling points in the field of LiFi technology. In the future, up to 350 students will be able to benefit from this advanced technology.

     

    Modernizing the school day with Trulifi

    "Earlier this summer, we began to equip classrooms with Trulifi by Signify and it has completely replaced the Wi-Fi in these rooms. Data transmission is stable and fast. Even in large classes, the faculty can use it for presentations and the students can use it for research, " said Esther Knoblich, the school’s Managing Director. "The switch from cable or WiFi to LiFi went smoothly, and the faculty could use the new system without having to sit through an elaborate technical introduction. We are particularly pleased that classes now have network access for individual lessons, which remain exclusively within the classroom."

    Comprehensive connectivity is essential for the school day of the future. With this in mind, we are very pleased to introduce cutting edge technology into the classroom together with the Freie Waldorfschule am Prenzlauer Berg.”

     

    Olivia Qiu
    Chief Innovation Officer for Signify

    Suitable in many domains

    In a world full of online meetings, live streaming, social media, and gaming, Internet connectivity and data communication must be fast, secure, and reliable. Trulifi by Signify, ensuring high-speed connectivity through light, is the perfect solution. Trulifi can also be retrofitted in existing Philips luminaires or installed as a single system.

     

    Trulifi by Signify is highly suitable for use in government, education aerospace and in other areas where wireless connectivity is poor, unavailable, or restricted. LiFi is a technology based on line of sight, making it impossible to eavesdrop or hack into the LiFi network from another room or from outside the building, or hinder the wireless communication.

     

    Curious about how Trulifi by Signify can benefit your organization? Visit our webpages.

    For further information, please contact:

    Signify Trulifi Marketing & Communications

    Floris Maassen

    Tel: + 31 6 48509129

    E-mail: floris.maassen@signify.com

    About Signify

     

    Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.
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
    • Signify starts EUR 150 million share repurchase program

      February 04, 2025

      Signify starts EUR 150 million share repurchase program