Eindhoven, the Netherlands – Signify (Euronext: LIGHT), the world leader in lighting, is launching new home monitoring technology and software features to complement its WiZ smart lighting system, pairing lighting and security in a simple, smart and secure way. The new WiZ indoor camera combines with software updates on the WiZ app, WiZ lights and SpaceSense motion detection technology to create an integrated solution that give users peace of mind when away from home.
Using the power of light and motion detection to deter intruders
WiZ integrates home monitoring features in its smart lighting system, taking advantage of the fact that lights are found throughout the home and can be one of the most effective tools to discourage potential intruders. With a seamless user experience in mind, the WiZ app is optimized with intuitive features, such as customizable monitoring routines, allowing users to both control their lighting and monitor their home with a single tap in the app. They simply click on their desired routine to let the WiZ system know they are going away and activate a set of lighting behaviors to help secure their home.
The WiZ app can now also notify users of unexpected activity in their home, allowing them to take immediate action. With SpaceSense motion detection technology, every compatible WiZ light is a motion sensor that detects movement in the coverage area. The award-winning technology makes the WiZ smart ecosystem one of the most comprehensive, and when combined with the new WiZ indoor camera, the system provides full coverage for the entire home. Consumers can activate WiZ monitoring for the entire home or for certain areas only and can quickly turn it off when necessary.
WiZ lights can also be automated with presence simulation: they will turn on and off automatically to simulate the presence of somebody at home. Users can decide how the lights will react when motion is detected: turn on to full brightness, flash, or display vibrant colors, for example.
Danny Lousberg
Head of Software Product Management WiZ
WiZ indoor camera to keep an eye on users’ homes
An important element of the new home monitoring solution is the WiZ indoor camera. It will allow consumers to control and see what’s always happening at home and will also notify them of any suspicious movement or sound. As soon as users receive a notification, they can open the WiZ app to get a live view of what’s going on.
The WiZ indoor camera is equipped with night vision, which is automatically enabled when the light level is low enough, using infrared to light up the space and ensure clear visibility. The image-based motion detection can also pick up on any sudden loud noises, such as the breaking of windows or fire/smoke alarms, and send notifications. Additional features include two-way audio feature, wide 120 degree viewing angle, full HD, and an SD card slot.
Those new to the WiZ ecosystem can begin their home monitoring journey with the home monitoring starter kit, composed of the new WiZ indoor camera and WiZ lights. WiZ will provide an optional subscription service to unlock additional features, like the option of storing media from the WiZ indoor camera in the cloud for up to 30 days, defining motion activity zones and/or privacy zones in selected areas, or starting a manual recording while the WiZ camera is streaming.
Availability
o RRP: EUR 89.99 / USD 69.99
o RRP: EUR 159.99
About WiZ Connected
WiZ Connected is an Internet of Things software solution provider focused on delivering easy-to-use, Wi-Fi-based smart lighting. Owned by Signify, the world leader in lighting, WiZ serves both consumer and professional markets in more than 70 countries. Learn more about WiZ Connected and how their innovative, connected lighting solutions make daily life easier at https://wizconnected.com.
Signify (Euronext: LIGHT) is the world leader in lighting for professionals, consumers and the Internet of Things. Our Philips products, Interact systems and data-enabled services deliver business value and transform life in homes, buildings and public spaces. In 2024, we had sales of EUR 6.1 billion, approximately 29,000 employees and a presence in over 70 countries. We unlock the extraordinary potential of light for brighter lives and a better world. We have been in the Dow Jones Sustainability World Index since our IPO for eight consecutive years and have achieved the EcoVadis Platinum rating for five consecutive years, placing Signify in the top one percent of companies assessed. News from Signify can be found in the Newsroom, on X, LinkedIn and Instagram. Information for investors is located on the Investor Relations page.
April 16, 2025
Signify completes share repurchases to cover share-based remuneration and continues with the share repurchases for capital reduction