Trulifi is complementary in locations where RF such as WiFi is not an option
By 2020, more than 50 billion devices will be connected to the internet, most of them wirelessly. This is placing wireless communication under increasing pressure. Put simply, the radio spectrum is becoming congested, with drop off and latency on the increase. Added to this is the growing use of data-heavy XR (AR, VR, MR) devices. For example, Virtual Reality is increasingly adopting industry standards such as 4K video and six DoF…and all this content needs to be sent over wireless networks. What’s more, there are more and more venues where RF wireless communication is not permitted due to security or safety.
Trulifi by Signify is the perfect solution. It’s a range of LiFi systems, providing fast, two-way wireless communication that’s reliable, secure and has the lowest latency for the first hop. Trulifi offers a fast 220 Mbps connection that can guarantee transmission of heavy data loads.
Trulifi also reduces cyber sickness, since it offers ultra-low latency and uses light waves to communicate. Interception is not possible as with radio-based communications; data in the room, stays in the room! And Trulifi is ideal in places where RF is not permitted or does not work.
Vuzix
Vuzix and Signify offer customers light based wireless connections with consistent high-speed, unique physical security to keep data safe and low latency for real time AR data streaming.
Conference Center High Tech Campus Eindhoven
Conference Center High Tech Campus hosts a variety of conferences and events. Having one of the conference rooms equipped with Trulifi was a natural thing to do.
Stirixis
Trulifi and Stirixis install LiFi at Pressious Arvanitidis in Maroussi, Greece for its fast, reliable, and secure wireless connectivity.