Kontich, Belgium – Exploring the possibilities of LED lighting design, Philips unveils a groundbreaking new design, redefining the essence of light. Lirio by Philips’ Piega Luce is a ultra-thinly folded pendent and wall light with a unique warm wood exterior. Inspired by nature and the simple form of a single folded sheet of paper, the sleek design of Piega Luce (made possible through innovative use of LEDs) transforms your home into a modern and sophisticated space.
Seamless light flow The Piega Luce provides a seamless flow of light from a minimalist body. Specifically designed to illuminate elongated features in the home, light flows from three edges of the slender Piega Luce, making it appear to float weightlessly in the air for a beautiful shadow effect in the home. The long-lasting warm white light powered by Philips LED technology can be easily dimmed to create a more intimate atmosphere. |
Minimalist earthbound design for inspirational living
The Piega Luce combines the best of European design and engineering. High quality aluminium is crafted to drape over a flexible LED core, and coated with a high quality walnut veneer. Piega Luce is available in warm American Walnut or Dark Smoke for a truly unique look
Trend alert: Wood minimalism – streamlined design is moving away from clinical colors and materials, instead embracing the comforting but contemporary look of natural, warm-toned wood.
Top tip: Suspend the Piega Luce over a long surface, such as a dining room table or kitchen counter, to add elegance to the space and highlight the sleek design. Use the Piega Luce to create a warm, intimate mood light when entertaining friends or simply enjoying the comfort of your home style. |
Recommended Retail Price: from €389
Lirio by Philips Piega Luce: Key Features
• The Piega Luce is ultra-thin only 16mm
• Special optical material distributes light uniformly
• The family consists of 2 pendants: 1400, 1100mm and one wall light
• Light output varies from 2400lm for the big pendant to 1900lm for the small pendant and 400lm for the wall light
• Made from high quality materials
• Long-lasting and flexible LED strips
• Available in American walnut or dark smoke wood
Name: Lena Segerdahl
Sector / department: Philips Consumer Lighting
Tel: +46 70 817 70 34
E-mail: lena.segerdahl@signify.com
Royal Philips (NYSE: PHG, AEX: PHIA) is a diversified health and well-being company, focused on improving people’s lives through meaningful innovation in the areas of Healthcare, Consumer Lifestyle and Lighting.
Headquartered in the Netherlands, Philips posted 2013 sales of EUR 23.3 billion and employs approximately 115,000 employees with sales and services in more than 100 countries. The company is a leader in cardiac care, acute care and home healthcare, energy efficient lighting solutions and new lighting applications, as well as male shaving and grooming and oral healthcare. News from Philips is located at www.philips.com/newscenter.